TLE52062SAKSA1 alternative

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
dpiazza
Level 1
Level 1
First question asked Welcome!

Hello everybody,
the TLE52062SAKSA1 component has been obsolete for several years, is there a functionally similar alternative? I could also evaluate formats formats (e.g. SMT).

Thanks

0 Likes
1 Solution
Sahil_K
Moderator
Moderator
Moderator
First like given 100 solutions authored 250 sign-ins

Hi @dpiazza,

For similar functionality, you can use IFX9201SG. However, some parameters are different from TLE5206-2S like: -

>>Package is PowerSO-12.

>>Min and max current are 6A and 8A respectively.

>>Operating voltage 4.5v-36v.

>>Also, output control is different( PWM/DIR).

>> It can support a max 11khz PWM and additionally support open load diagnosis.

Note:- It is not the exact replacement for the TLE5206-2S. so for your application please refer to the datasheet of the IFX9201SG.

Best Regards

Sahil Kumar

View solution in original post

0 Likes
1 Reply
Sahil_K
Moderator
Moderator
Moderator
First like given 100 solutions authored 250 sign-ins

Hi @dpiazza,

For similar functionality, you can use IFX9201SG. However, some parameters are different from TLE5206-2S like: -

>>Package is PowerSO-12.

>>Min and max current are 6A and 8A respectively.

>>Operating voltage 4.5v-36v.

>>Also, output control is different( PWM/DIR).

>> It can support a max 11khz PWM and additionally support open load diagnosis.

Note:- It is not the exact replacement for the TLE5206-2S. so for your application please refer to the datasheet of the IFX9201SG.

Best Regards

Sahil Kumar

0 Likes