- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I have this Board (REF-AIRCON-C302A-IM564) and I am trying to program it using keil uVision. I have some Queries which are stated as:
Query 1) Are there any examples for this board available in c language which can be used in keil uVision?
Query 2) Can I control All Motor Control Engine parameters using keil uVision?
Query 3) Can I run this Reference board with having all the Functionalities running for an actual outdoor Unit. Which means controlling of peripherals like Fan, 4 way Valves, Reading Ambient, Pipe, Exhaust Temperature, Sending and Receiving data between indoor and outdoor unit?
Regards,
Ali
Solved! Go to Solution.
- Labels:
-
ispn:30346:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Ali,
Query 1) Are there any examples for this board available in c language which can be used in keil uVision?
Yes,Please refer to code example in this link: IMC300A examples
Query 2) Can I control All Motor Control Engine parameters using keil uVision?
Not all the MCE parameters can be controlled using A-Core. Only dynamic parameters can be controlled using A-Core Please refer to JCOM Example in IMC300A examples for more details please refer to section 2.4 JCOM Inter-Chip Communication in iMOTION – MCE – Software Reference Manual v1.3
Can I run this Reference board with having all the Functionalities running for an actual outdoor Unit. Which means controlling of peripherals like Fan, 4 way Valves, Reading Ambient, Pipe, Exhaust Temperature, Sending and Receiving data between indoor and outdoor unit?
Yes, for more details please refer User Guide - REF-AIRCON-C302A-IM564
Please let us know if further support is needed.
Thanks,
Krupashankar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Ali,
Query 1) Are there any examples for this board available in c language which can be used in keil uVision?
Yes,Please refer to code example in this link: IMC300A examples
Query 2) Can I control All Motor Control Engine parameters using keil uVision?
Not all the MCE parameters can be controlled using A-Core. Only dynamic parameters can be controlled using A-Core Please refer to JCOM Example in IMC300A examples for more details please refer to section 2.4 JCOM Inter-Chip Communication in iMOTION – MCE – Software Reference Manual v1.3
Can I run this Reference board with having all the Functionalities running for an actual outdoor Unit. Which means controlling of peripherals like Fan, 4 way Valves, Reading Ambient, Pipe, Exhaust Temperature, Sending and Receiving data between indoor and outdoor unit?
Yes, for more details please refer User Guide - REF-AIRCON-C302A-IM564
Please let us know if further support is needed.
Thanks,
Krupashankar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Krupashankar,
Thank you for your response.
So I did install keil mdk537 and tried to build the code (example UART) but at first it was giving error of uVision 5 is needed then I did installed the uVision 5 Support with that I changed the Arm compiler to 5.06 and was having issues with license, server etc.
Again Changing the compiler to 6.18 it is giving these errors
What should I do?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Can you please follow the solution provided in the link below
Best Regards