Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Naveenkongari
Level 1
Level 1
First question asked Welcome!

I am trying to implement UART FIFO Mode protocol implementation in IMD111T-F040 Microcontroller. I taken the this pdf as reference(Infineon-AN2021-10_How_to_Use_iMOTION_Configurable_UART-ApplicationNotes-v02_00-EN). This pdf has FIFO and Buffer mode protocol implementation sample programs but we don't have pin configuration details. So, while i am trying to implement the FIFO Mode the data transmit from microcontroller is working. But whatever data is i sent to microcontroller the interrupt is not generating(data receiving is not not happening). So can you please answer my questions Questions: 1. can I enable or disable solution designer com port? 2. can I declare Tx and Rx pin configuration(Input or Output)? 3. currently i am using FW 5.03.07. So is UART support or not in this version?

0 Likes
1 Reply
Viswa
Moderator
Moderator
Moderator
10 likes received 50 solutions authored 100 replies posted

Hi 

1) Yes, As there is only one UART in IMD111T device the UART can be used as either USER UART or Solution Designer COMM UART( programming)

2) No, It is preconfigured and only the dedicated pin can be used

3) Yes USER UART is supported

Best Regards

0 Likes