Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Hello,

I'm having a hard time controlling RPM.

I set the RPM to 2000 RPM when I set it.
However, there is a symptom that the RPM does not exceed 1000 and continues to go down.

I've modified several parameters for this symptom, but it never improved.

If you are aware of this problem, please reply.

0 Likes
1 Solution
RupakC
Moderator
Moderator
Moderator
100 solutions authored 250 sign-ins 25 likes received

Hello @JasonLEE 

The issue in this case is not related to shunt configuration. The load on the motor was too high such that the current drawn was exceeding the 5A limit that was set within the MCE Wizard. Increasing the current limit in software was able to solve this issue. 

Regards

RupakC

View solution in original post

0 Likes
49 Replies
喜马拉雅之雪
Employee

Hi:

Would you share that what time your motor can't run to high speed and your design? The output is open load or...?

0 Likes
lock attach
Attachments are accessible only for community members.
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Hi,

What kind of design should I share?

It uses EVAL-IM818LCC and EVAL-IM828XCC development boards.

 

0 Likes
喜马拉雅之雪
Employee

What kind of load of IM818 and 828 board?

Did you have and share there motor drive current waveform by MCEWizard?

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

How should I measure the motor load?
I've got an impeller.

Is there a waveform in MCEWizard?
If I have a waveform, which waveform should I share?

0 Likes

As there waveform are from soft "read", you can dubg your setup(MCEWizard) with system.

0 Likes
喜马拉雅之雪
Employee

Hi:

Would you share the project detailed information?

From your comments, we get out you testng IM818 and IM828 board. But there are  power boards and they can do most function. we don't know that about what's your project and you want.

For waveform, you can gat out MCEDesigner:

_0-1672104410144.png_1-1672104503299.png

 

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Hi,

 

IM828XCC Single Shunt's no-load waveform.

I set it to 250 RPM.

1.png

2.png

3.png

   

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

IM828XCC Leg Shunt's no-load waveform.

I set it to 250 RPM.

 

11.png

22.png

33.png

   

0 Likes
lock attach
Attachments are accessible only for community members.
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Our system is for FAN motor for HVAC.
The waveform you just measured was tested with a customized board.

Backemf and all parameter values were accurately measured.

I attached the .mc2 file, so please check it.

 

 

 

0 Likes
喜马拉雅之雪
Employee

What's kind of your board?

EVAL-M1-IM828-A is single shunt solution.

EVAL-M1-IM818-A is leg shunt solution.

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Hi, @喜马拉雅之雪 

1. I have both EVAL boards.

EVAL-M1-IM828-A is single shunt solution.

EVAL-M1-IM818-A is leg shunt solution.

2. We also have two customized boards with the same design.

0 Likes
喜马拉雅之雪
Employee

For IM818-A board, as motor poles setup  is 20, so the drive target is 333Hz.

Would you try different setup with No.58/60/94 question?

My forvert is:

   Fiux estimator time constant: 3~7msec,

  Gatekill filter time constant:1uS.

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Hi, @喜马拉雅之雪 

My motor pole is 10P.

20P is set incorrectly.

Can you provide a solution based on 10P?

Q58) What value should I set for this part?

I need a maximum of 2500 RPM.

0 Likes
喜马拉雅之雪
Employee

Happy new year

1) Would you please best setup there question.

2) 3~7mS can meet 10P application.

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Hi @喜马拉雅之雪 

In case of Q58, I didn't know how, so I left it there
The rest were set up as you provided the solution, but the problem did not improve.

0 Likes
喜马拉雅之雪
Employee

1) What's your power input? AC380V or ...

2) Could you test the motor KV value?

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

1) AC 3 Phase 380V.

2) Could you tell me how to measure the motor KV value?

0 Likes

Have you a digital oscilloscope?

If OK, OSC probe connect to motor pin: U-V.

Rotating the motor at a constant speed, test U-V pin voltage waveform by OSC. Intercept the waveform and upload.

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Hi.

Two methods were measured using an oscilloscope.

1) U, V phase is measured in detail with an oscilloscope.
RPM is 200.
This is rotated by the motor driver.

2) U phase was measured in Oscilloscope.
This part rotates consistently by hand.

1.jpg

2.png

  

  

 

0 Likes
喜马拉雅之雪
Employee

Could you zoon in the waveform for read the voltage and frequency?

_0-1672193670231.png

 

0 Likes
喜马拉雅之雪
Employee

The motor is Y connect? The waveform is U to three-phase midpoin?

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

The motor connection is a Y connection.

The waveform is a U-V connection.

Put a scope on the U
I have connected a GND to V.

 

scope.jpg

scope2.jpg

0 Likes
喜马拉雅之雪
Employee

Would you please double check the DC BUS voltage? From your waveform, it is DC290V.

_0-1672197035153.png

 

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

안녕,

다시 측정했습니다.
확인해주십시오.

 

scope3.jpg

 

scope4.jpg

0 Likes

Would you please check your test system. The waveform is different of standard.

This is typical of the switching waveform of EVAL-M1-IM818/828-A @AC380V 3-phase input:

_1-1672201769669.png

 

0 Likes
喜马拉雅之雪
Employee

? DC270V?

_0-1672201356227.png

 

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

This is DC 600V.

Not 270~300.

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Could you tell me where and how you checked the waveform? I will check the same way.

0 Likes
喜马拉雅之雪
Employee

If BUS is DC600V, the waveform is not right.

Could you made the testing picture/photo (include probe and OSC )?

0 Likes
喜马拉雅之雪
Employee

Thanks for your testing and waveform. The motor is Ke=132.7V/krpm.

The motor Vp-p@2000rpk=265V*2*1.414=375V

DC BUS: Vbus=Vp-p/((T-2td)/T)=399V

So if DC BUS is high than DC400V, the motor can go to 2000rpm.

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

테스트한 보드는 EVAL 보드가 아닌 맞춤형 보드입니다.
그러나 디자인은 EVAL 보드와 같습니다.

범위는 U, V, W 섹션에서 측정되었습니다.
잘못된 사항이 있으면 알려주세요.   

KakaoTalk_20221228_140105517.jpg

KakaoTalk_20221228_140105517_01.jpg

SCOPE5.png

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

The motor is Ke=132.7V/krpm.

The motor Vp-p@2000rpk=265V*2*1.414=375V

DC BUS: Vbus=Vp-p/((T-2td)/T)=399V

So if DC BUS is high than DC400V, the motor can go to 2000rpm.

 

I don't know if this value is correct.
The motor's symptoms have not improved at all.
It's the same.

RPM does not go up.

0 Likes
喜马拉雅之雪
Employee

I understand that your testing. However, don't floating the ground of the probe.

I think about,this is only testing skill, it's not big problem.

Could you tall me about what's your ran of max speed?

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

The maximum speed I want is 2500 RPM.

But it only goes up to 1000 RPM.
It's not going up any more.

Can't you solve this problem?

 

Where should the grounding of the probe be located?

0 Likes
喜马拉雅之雪
Employee

My favort is power ground(-bus) with PWM power waveform. Other testing, I like use local ground(test reference ground is nearest the test target).

For 850rpm, could you test current and PWM waveform?

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Which part are you talking about if it's local ground?

Can you explain it in more detail?

Are you talking about the Earth part?

0 Likes
喜马拉雅之雪
Employee

MCU and shunt picture... 

For example, shunt wavefrom:

This is test via layout with the shunt resistance:

_0-1672211481247.png

Probe:

_1-1672212280913.png

 

 

0 Likes
JasonLEE
Level 5
Level 5
100 replies posted 250 sign-ins First like received

Tested as you told me and exploded.

The whole hardware exploded.

d.jpg

0 Likes
喜马拉雅之雪
Employee

WOW! DEEP LAMENT...

Could you share the shunt resistance part number? And shunt AMP loop SCH?

0 Likes