Announcements

Join us for FREE at OktoberTech Asia Pacific and hear about decarbonizing future mobility. Click here for more details.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Motor Control ICs Forum Discussions

User17942
Level 1
First question asked
Level 1
Hello!

I am using the IMC101T-F064 integrated circuit in one development and want to use the latest software. In the "Software" section there is a link to the [ IMC101T-F064 MCE Software Package v1.2.1 ] archive with new configuration files for the IMC101 product, but in the inside of the archive there are files for the IMC102 product !!! Please tell me where to get the new configuration files for the product IMC101?
Thank.
0 Likes
1 Reply
User12531
Level 1
Level 1
Hi Merlin,

Thank you for the hint.

Please click on the following MCE_IMC101T-F064_v01_02 download link:
IMC101T-F064 MCE Software Package v1.2.1

This MCE software was tested, using the following environment.
• Control Board: EVAL-M1-101T
• Power Board: Eval-M1-05-65D
• Motor Specification: 8Pole, 0.4A R=38.5ohm, Lq= 196mH, Ld=196mH, Ke= 36V, 2730 RPM
0 Likes