- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am using EVAL-M3-302F I want to run simple program Blink led. I tried compile but there is error in IMC300A.h header file & imc300a_port1.h header file. I am beginner in Imotion have a background of Arduino programming where lot of example & doc available.
my understanding is I have to call function from program write,set,read port bits
write_PORT1_PortControlForPort0Pin8_IOCR8(PORT1_PC8_Output_PushPull__Generalpurpose_output);/*P0.8, set as output*/
but if header file have error I cant solved it.
Build started: Project: IMC302A_UART
*** Using Compiler 'V6.18', folder: 'C:\Keil_v5\ARM\ARMCLANG\Bin'
Build target 'Target 1'
main.c(3): error: expected "FILENAME" or <FILENAME>
**********************************************************************************************************************/
^
main.c(4): warning: In file included from...
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\IMC300A.h(60): warning: commas at the end of enumerator lists are a C99-specific feature [-Wc99-extensions]
SysTick_IRQn = -1, /*!< 15 System Tick Timer */
^~
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\IMC300A.h(191): warning: anonymous unions are a C11 extension [-Wc11-extensions]
union {
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\IMC300A.h(443): warning: anonymous unions are a C11 extension [-Wc11-extensions]
union {
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\IMC300A.h(452): warning: anonymous unions are a C11 extension [-Wc11-extensions]
union {
^
main.c(6): warning: In file included from...
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(27): warning: In file included from...
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_library.h(24): warning: non-portable path to file '<IMC300A.h>'; specified path differs in case from file name on disk [-Wnonportable-include-path]
#include <imc300a.h>
^~~~~~~~~~~
<IMC300A.h>
main.c(6): warning: In file included from...
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(43): error: unknown type name 'inline'
static inline void write_PORT1_OUT( uint32_t out )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(48): error: unknown type name 'inline'
static inline uint32_t read_PORT1_OUT( void )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(48): error: expected ';' after top level declarator
static inline uint32_t read_PORT1_OUT( void )
^
;
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(63): error: unknown type name 'inline'
static inline void write_PORT1_Port1OutputBit0_OUT( PORT1_OUT_P0_t p0 )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(63): error: unknown type name 'PORT1_OUT_P0_t'
static inline void write_PORT1_Port1OutputBit0_OUT( PORT1_OUT_P0_t p0 )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(69): error: unknown type name 'inline'
static inline void setbit_PORT1_Port1OutputBit0_OUT( void )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(74): error: unknown type name 'inline'
static inline void clearbit_PORT1_Port1OutputBit0_OUT( void )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(79): error: unknown type name 'inline'
static inline uint32_t read_PORT1_Port1OutputBit0_OUT( void )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(79): error: expected ';' after top level declarator
static inline uint32_t read_PORT1_Port1OutputBit0_OUT( void )
^
;
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(94): error: unknown type name 'inline'
static inline void write_PORT1_Port1OutputBit1_OUT( PORT1_OUT_P1_t p1 )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(94): error: unknown type name 'PORT1_OUT_P1_t'
static inline void write_PORT1_Port1OutputBit1_OUT( PORT1_OUT_P1_t p1 )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(100): error: unknown type name 'inline'
static inline void setbit_PORT1_Port1OutputBit1_OUT( void )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(105): error: unknown type name 'inline'
static inline void clearbit_PORT1_Port1OutputBit1_OUT( void )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(110): error: unknown type name 'inline'
static inline uint32_t read_PORT1_Port1OutputBit1_OUT( void )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(110): error: expected ';' after top level declarator
static inline uint32_t read_PORT1_Port1OutputBit1_OUT( void )
^
;
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(125): error: unknown type name 'inline'
static inline void write_PORT1_Port1OutputBit2_OUT( PORT1_OUT_P2_t p2 )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(125): error: unknown type name 'PORT1_OUT_P2_t'
static inline void write_PORT1_Port1OutputBit2_OUT( PORT1_OUT_P2_t p2 )
^
C:/Users/HP/AppData/Local/Arm/Packs/Infineon/IMC300A_DFP/1.1.0/Device/IMC300_series/Include\imc300a_port1.h(131): error: unknown type name 'inline'
static inline void setbit_PORT1_Port1OutputBit2_OUT( void )
^
fatal error: too many errors emitted, stopping now [-ferror-limit=]
5 warnings and 20 errors generated.
compiling main.c...
".\Objects\IMC302A_UART.axf" - 19 Error(s), 5 Warning(s).
Target not created.
Build Time Elapsed: 00:00:01
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @sohail,
The IMC300A example code is supported in
MDK Version : 5.36
compiler : V5.06 update 7(build 960)
Code example is developed based on ARM Compiler 5 so it is not supported in higher compiler version ( ARM Compiler 6) please follow this document: Migrate ARM Compiler 5 to ARM Compiler 6 to build the code example in higher compiler version.
Thanks,
Krupashankar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @sohail,
The IMC300A example code is supported in
MDK Version : 5.36
compiler : V5.06 update 7(build 960)
Code example is developed based on ARM Compiler 5 so it is not supported in higher compiler version ( ARM Compiler 6) please follow this document: Migrate ARM Compiler 5 to ARM Compiler 6 to build the code example in higher compiler version.
Thanks,
Krupashankar