- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have an EVAL-M1-301F, I have got my motor running fine. I tried to set UART1 up as User mode but failed and I'm not sure why. So I set up UART0 as user mode and can now successfully control the motor using the basic protocol. However I have now come to change the parameters through MCEDesigner (generated through MCEWizard) and realised this is now impossible.
I have tried hooking up a USB-serial port adapter to UART1 (J9) to get debug access through that as MCEWizard would seem to suggest but that UART is dead. Rx and Tx floating.
What is the quickest / easiest way to recover debug access?
Thanks Jonathan
Solved! Go to Solution.
- Labels:
-
ispn:28121:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Joni,
Please refer to this KBA for Switching UART mode: Switch UART mode for iMotion devices - KBA235121
Hope this solves the issue and please let us know if any further clarification is needed.
Thanks,
Krupashankar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Joni,
Please refer to this KBA for Switching UART mode: Switch UART mode for iMotion devices - KBA235121
Hope this solves the issue and please let us know if any further clarification is needed.
Thanks,
Krupashankar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks Krupashankar
That has allowed me to restore the debug to UART0.
However I still cannot seem to get get both the UART0 running in "Debug" mode and UART1 running in "User" mode at the same time. I am using the following settings in MCEWizard 2.3.0.0:
UART Node Address = 1
User UART Function Definition = UART1
UART Baud Rate = tried both 57600 and 115200
UART Tx Delay = 0
Communications between MCU and MCE cores = Disable
I'm connecting an isolated USB->UART adaptor to pins 1,3,4 on J9!
Does this sound correct?
Thanks
Jonathan