Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Motor Control ICs Forum Discussions

Lauriv
Level 1
First solution authored First reply posted First question asked
Level 1

Hi, I have tried to run DB59C024035R-B3 brushless-dc motor with EVAL-M1-101TF/EVAL-M1-05F310R, but I'm getting instant Gatekill/low dc voltage fault every time in MCEdesigner. I'm not sure even if this motor is supposed to work with those parts. 

Does someone have any ideas on how to investigate this? Or could someone point out what motor would work properly with EVAL-M1-101TF/EVAL-M1-05F310R? 

 

I am using IMC101T-F048 MCE Software Package v1.3.3. 

0 Likes
1 Solution
Lauriv
Level 1
First solution authored First reply posted First question asked
Level 1

Hi,

I got it working changing gatekill source to gatekill pin. I'm not sure how safe that is but now it is working.

I added parameter file. 

This case can be closed. 

Thank you,

Lauri

View solution in original post

0 Likes
6 Replies
Krupashankar
Moderator
Moderator 250 replies posted 100 solutions authored 5 likes given
Moderator

Hi @Lauriv,

Thanks! for posting in the Infineon Community.

EVAL-M1-05F310R - Nominal input voltage 30 ~ 72 Vdc

From the Datasheet of the motor, we could see the rated voltage of the motor is 24V.

Could you please share the configuration .mc2 file? This will help us to understand the issue better.

 

Thanks,

Krupashankar

 

0 Likes
Lauriv
Level 1
First solution authored First reply posted First question asked
Level 1

Hi,

I used file below, just changed poles count.

https://www.infineon.com/dgdl/Infineon-MCEWizard_Configuration_Files-DevelopmentTools-v01_01-EN.zip?...

"The file type (.mc2) is not supported. Valid file types are: jpg, gif, png, json, doc, pdf, xls, docx, html, htm, xlsx, pptx, zip."

Should I look for motor that is between 30-72 or is there some work around?

Thank you,

Lauri

0 Likes
Lauriv
Level 1
First solution authored First reply posted First question asked
Level 1

Ah, found it.  .mc2 file is inside zip file

0 Likes
Krupashankar
Moderator
Moderator 250 replies posted 100 solutions authored 5 likes given
Moderator

Hi @Lauriv,

Based on your attached .mc2 file We could find that motor parameters don't match with the configuration(.mc2)

Could you please update all the parameters based on the motor datasheet? and let us know if you are able to run the motor.

 

Thanks,

Krupashankar 

0 Likes
Lauriv
Level 1
First solution authored First reply posted First question asked
Level 1

Hi,

I got it working changing gatekill source to gatekill pin. I'm not sure how safe that is but now it is working.

I added parameter file. 

This case can be closed. 

Thank you,

Lauri

0 Likes
Krupashankar
Moderator
Moderator 250 replies posted 100 solutions authored 5 likes given
Moderator

Hi @Lauriv,

This will disable the gate kill fault triggered from the comparator due to overcurrent. Please make sure your gatekill pin triggers at the time of over current

 

Thanks,

Krupashankar

0 Likes