- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
We developped a specific power PCB to drive a Brushless Motor (34KV and 20KW)
Specifications in datasheet are :
No. of Pole : 62
Arms : 3.7A
Rated Speed : 34 RPM/V (I try with 25V)
Line to Line Resistance : 0.008Ohms
Line to Line Inductance : 0.008mH
Configuration file is attached to the post
Here is a video of the motor try to run: Oscillation_Video
-We put a 500rpm value set. But the motor oscillate between 200 and 600rpm
-The start of the motor is a little bit difficult.
Our schematic is the same than EVAL-M1-05F804R except these values :
-amplification part of the shunt : R18=1KOhms / R30=1220Ohms / R26=5412Ohms.
Do you have some ideas on how to solve these oscillations behavior ?
Regards,
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @seb_44120
First of all, you need need to verify that all parameters are correct. I found the following parameter incorrect (Compare your motor parameters with the .mc2 file) :
1. Here is the phase R&L, so it is half of Line to Line
Line to Line Resistance : 0.008Ohms
Line to Line Inductance : 0.008mH
These parameters are 0.004Ohms, 0.004mH.
For more motor parameters measure and input, you can refer this manual:how to measure motor parameters
2. For current measurment. R18=1KOhms / R30=1220Ohms / R26=5412Ohms.
OP gain G ≈ (R18+R19+R20)/(R19+R20) = (1000+590+47)/(590+47) =2.57
IU+ voltage: VIU+ = R16*I*G = 12.85mV/A
Voltage offset: Vo = R30/(R26+R29+R30)*3.3 V = 1220/(5412+10+1220) *3.3V = 0.606V
There is offset circuit on IMC101TF board:
So, Current scaling = 12.85*0.833mV/A = 10.7mV/A
These two parameters need modify on your MCEWizard .
The current scaling is very low, and the rated amps is 3.7A, internal current gain is 1. So that the current ADC value is very low, The noise interference will be serious. You can modify the internal gain 1 to 3 or higher. Or modify hardware : Increase OP gain / Increase R shunt.
3. For current measurment adjustment. First you can refer this EVAL-M1-IM535-UserManual page 13-15, use “VF Diagnostic” function in MCEDesigner. Check whether the current HW and parameters are allright.
4.Use single shunt, You selected Phase Shift mode current sensing, you should tune the Q86 and Q90 values.
For more detail information of current sensing, you should refer Software Reference Manual 2.1.7.2 Single Shunt Current Measurement and4.1 How to check if the current sensing setup is good.
5. For Motor Tuning problems, suggestion refer Chapter 4 of Software Reference Manual .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @seb_44120
First of all, you need need to verify that all parameters are correct. I found the following parameter incorrect (Compare your motor parameters with the .mc2 file) :
1. Here is the phase R&L, so it is half of Line to Line
Line to Line Resistance : 0.008Ohms
Line to Line Inductance : 0.008mH
These parameters are 0.004Ohms, 0.004mH.
For more motor parameters measure and input, you can refer this manual:how to measure motor parameters
2. For current measurment. R18=1KOhms / R30=1220Ohms / R26=5412Ohms.
OP gain G ≈ (R18+R19+R20)/(R19+R20) = (1000+590+47)/(590+47) =2.57
IU+ voltage: VIU+ = R16*I*G = 12.85mV/A
Voltage offset: Vo = R30/(R26+R29+R30)*3.3 V = 1220/(5412+10+1220) *3.3V = 0.606V
There is offset circuit on IMC101TF board:
So, Current scaling = 12.85*0.833mV/A = 10.7mV/A
These two parameters need modify on your MCEWizard .
The current scaling is very low, and the rated amps is 3.7A, internal current gain is 1. So that the current ADC value is very low, The noise interference will be serious. You can modify the internal gain 1 to 3 or higher. Or modify hardware : Increase OP gain / Increase R shunt.
3. For current measurment adjustment. First you can refer this EVAL-M1-IM535-UserManual page 13-15, use “VF Diagnostic” function in MCEDesigner. Check whether the current HW and parameters are allright.
4.Use single shunt, You selected Phase Shift mode current sensing, you should tune the Q86 and Q90 values.
For more detail information of current sensing, you should refer Software Reference Manual 2.1.7.2 Single Shunt Current Measurement and4.1 How to check if the current sensing setup is good.
5. For Motor Tuning problems, suggestion refer Chapter 4 of Software Reference Manual .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for your question.
From your discuss, I think that about your system had been shake.
Would you please change "Current regulator bandwidth" to between 200~1700 and try again.
Thanks & Regards