Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Motor Control ICs Forum Discussions

kkkkjeong
Level 1
Level 1
5 questions asked 5 sign-ins 5 replies posted

Hi i am using EVAL M3 IM564 and EVAL M3 102T.

QUESTION 1
I want to run using UART.

So, first i send a message to MCE
(01 06 01 20 00 00 FE D9)

And i sent a message to operate at 3000rpm
like below.

01 03 00 00 b8 0b 47 f1

But operation is different that using ISD.

ISD is good condition.(3000rpm)
UART is working and then it stops.(2000rpm->stop)

why is it that?

QUESTION 2
Where are parameter lists?

I can't find it.

kkkkjeong_0-1678781515157.png



Thank you at all times.

 

0 Likes
1 Solution
Krupashankar
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @kkkkjeong,

1) The USER UART protocol in section 2.3 User Mode UART of document iMOTION™ Motion Control Engine
Software Reference Manual is for Firmware version V1.03.03

This protocol snippet is valid only with MCE Designer and MCE wizard for older firmware version V1.03.03.

Can you please tell us what do you mean by ISD is it iMOTION Solution Designer?

2) Parameter list and register ID is present in document iMOTION™ Motion Control Engine Software Reference Manual:

  •  Section 3.2 Motor Control Register.
  •  Section 3.1 System Control Register
  • Section 3.3 PFC Control Register
  • Section  3.4 Script Register 

Index represents the register ID.

3) iMOTION supports multiple parameter to control different set of motors and hardware configurations, Parameter set number can be set from MCE Wizard Ques 31 Parameter Set Number.

For more details please refer to application note AN2020-25 Handling multiple motor parameters with iMOTION™2.0 

 

 

Thanks,

Krupashankar

View solution in original post

0 Likes
3 Replies
Krupashankar
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 5 likes given

Hi @kkkkjeong,

1) The USER UART protocol in section 2.3 User Mode UART of document iMOTION™ Motion Control Engine
Software Reference Manual is for Firmware version V1.03.03

This protocol snippet is valid only with MCE Designer and MCE wizard for older firmware version V1.03.03.

Can you please tell us what do you mean by ISD is it iMOTION Solution Designer?

2) Parameter list and register ID is present in document iMOTION™ Motion Control Engine Software Reference Manual:

  •  Section 3.2 Motor Control Register.
  •  Section 3.1 System Control Register
  • Section 3.3 PFC Control Register
  • Section  3.4 Script Register 

Index represents the register ID.

3) iMOTION supports multiple parameter to control different set of motors and hardware configurations, Parameter set number can be set from MCE Wizard Ques 31 Parameter Set Number.

For more details please refer to application note AN2020-25 Handling multiple motor parameters with iMOTION™2.0 

 

 

Thanks,

Krupashankar

0 Likes

1) Yes ISD is imoction solution designer.


01 03 00 00 b8 0b 47 f1
Is this frame 3000 rpm control?
b8 0b(low, high) = >  3000

2,3) I got it. Thank you.

 

0 Likes

I solved that.

The relevant information was here.
0x3fff(16383) = 100%

iMOTION™ Motion Control Engine Software Reference Manual:

kkkkjeong_0-1678856885508.png

 

0 Likes
This widget could not be displayed.