Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

ModusToolbox™ Forum Discussions

ClarkJarvis
ModusToolbox™
ModusToolbox™ v3.2 is now available for installation using the new ModusToolbox™ Setup program.  ModusToolbox™ provides an adaptable work environment ... Show More
ClarkJarvis
ModusToolbox™
ModusToolbox™ v3.2 is now available for installation using the new ModusToolbox™ Setup program.  ModusToolbox™ provides an adaptable work environment ... Show More
GuoXiangH_21
ModusToolbox™
                                                      ModusToolbox补丁安装指南           补丁及文档请从此贴附件中下载 安装ModusToolBox 3.1 (ModusToolbox_3.1-windows-install.exe... Show More
Jedison
ModusToolbox™
Dear forum, I have a problem uninstalling Modus Toolbox Software 3.2.0.16028. The situation: I installed the ModusToolbox Setup 1.0.0 and Modus Toolbo... Show More
Balek
ModusToolbox™
Hi, Whenever I open a MTB project, I get a command line terminal getting launched as well. Is there a way to fix this issue? I am using MTB v3.0. I am... Show More
chriswbowers
ModusToolbox™
I cannot complete installation of ModusToolbox. It says that Login is required to complete installation, but login fails. This is with ModusToolbox Se... Show More
YuMa_1534086
ModusToolbox™
Hi Infineon.   I think that Modus supports double of data type(double precision floating point number type). Which file in Modus defines about double?... Show More
Koumak_v2
ModusToolbox™
Hi all, I would like to try the firmware upgrade example for my dev kit. But it is not working.   Can you please advise me what I have wrong? I am at... Show More
alexfanq
ModusToolbox™
I would like to use Modustoolbox to develop rt thread project and was trying to follow the guide https://community.infineon.com/t5/Knowledge-Base-Articles/Porting-RT-Thread-to-ModusToolbox/ta-p/664401... Show More
Translation_Bot
ModusToolbox™
I am writing a program for a BLE HID device and I want to call the functions in the file mtb_shared/btstack/release-v3.8.2/wiced_include/wiced_bt_hidd... Show More
YuMa_1534086
ModusToolbox™
Hi Infineon.   PSoC Creator allows flash protection with “Design Wide Resources(Flash Security)”. Please confirm below figure.       Could you please... Show More