Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

ModusToolbox™ Forum Discussions

ClarkJarvis
ModusToolbox™
ModusToolbox™ v3.2 is now available for installation using the new ModusToolbox™ Setup program.  ModusToolbox™ provides an adaptable work environment ... Show More
GaryS_06
ModusToolbox™
Check out this webinar on low-power system design featuring PSoC 6 and the CYW43012 done by our Apps team: JayaB_71​ and MeenakshiR_71​https://event.on24.com/wcc/r/2341379/7FA23146ADC03372DC776E269DA84183 Show More
YoIs_1298666
ModusToolbox™
Hello,In case of ModusToolbox1.1, I know that I was not able to select devices freely.Now, ModusToolbox is ver 2.1.Can I select device freely?Best reg... Show More
jama_4535901
ModusToolbox™
Good afternooncould you help me this is urgentI have 2 code with CYBT-213043-MESH1- It is a code that scans and can the mac adress or host of the devi... Show More
ErVe_4649071
ModusToolbox™
HelloI would like to know if you can help me with what I am looking to do.I am using the CYBT-213043-MESH evaluation kit, I already have a functional ... Show More
AaAa_4716276
ModusToolbox™
AWS IOT?
solved msg Solved
So AWS IOT supports MQTT. MQTT authentication uses certificates. What I know is for each device in order to communicate it must subscribe and before d... Show More
JaJa_4715126
ModusToolbox™
Hi friends,as I recently had problems to run the code example CE229112 (PSoC6+WiFi TCP Client), I figured out that Python access to Wifi was blocked p... Show More
gali_925661
ModusToolbox™
I am using the BLE063 kit which comes with a pre-configured UART channel at P5_0 and P5_1. I would like to know how can I create another UART channel ... Show More
Kenshow
ModusToolbox™
Hello,I am using Modus toolbox2.1 with PSoC6 BLE Pioneer kit.If the compiler optimization options are changed, the following methods described in KBA229177 ... Show More
WiWi_4702256
ModusToolbox™
When I first start up... It can take up to 5 minutes to respond.Also, when I am reading something on community, come back, open,close a file, it hangs... Show More
Kenshow
ModusToolbox™
Hi,Is this a known issue for Modus toolbox2.1?I encountered a bug in MTG 2.1 as follows:When I copy a project in Project Explorer (Ctrl + c and Ctrl +... Show More