Hi,
During compilation I got this error from /mtb_shared/mbedtls/mbedtls-2.22.0/include/mbedtls/check_config.h
I have no idea why I would get an error from a file inside mtb_shared?
I tried both ModusToolbox 2.2 and ModusToolbox 2.3 and they are the same.
The file looks like this:
Thanks!
Can you let me know which specific project are you compiling?
I was building the Hello World project but with a custom BSP. The chip set I use is exactly the same as CY8CPROTO-062-4343W.
The original example project SPI_Master for CY8CPROTO-062-4343W could be built finely?
It looks there is line in your project makefile -
COMPONENTS=FREERTOS PSOC6HAL LWIP MBEDTLS 4343W
Is this line neccessary?
The original example project was built ok. I need to use the custom BSP and going to add Wi-Fi capabilities. That's why I added those components in the makefile. I've used this method (starting from an example project and then create my custom BSP) with ModusToolbox 2.2 for more than half a year. It's always been working. It gave me this error just recently.
Is there some update happening on the mtb_shared file in the background?
I tried your project and also has some compiling errors, but the errors are not same with you.
Can you add the additional codes step by step based on the bare example code, and to see the error generated on which step/code line?