ModusToolbox™ General Forum Discussions
Hello Cypress!
At first, I want to say thank you for great modustoolbox.
Can you help me find the way configure wifi module. Also where I can find some examples with wifi module.
Thanks, Alex
Show LessHi,
I noted that debug cannot work with ModusToolbox/KitProg3 according to bellow Q&A,
Debugging not working with ModusToolbox/KitProg3
https://community.cypress.com/thread/43378
Answer:This is a known issue with older boards under Rev 13.
and I found that even programming successfully,LED also cannot blink,
is it known issue? does it also relate with board version.
I list my test environment for your reference.
Board:CY8CKIT-062-BLE Psoc 6 BLE pioneer board REV11
IDE:modus
Project:LED blink
Best regards.
Show LessHi,
I encountered bellow problems when used Modus 1.0 IDE.
Board:CY8CKIT-062-BLE
1.I enabled hex output according to ModusToolbox_IDE_User_Guide.pdf
page 44 Enable HEX File Generation,
but bellow message shown after I selected the HEX file generate by modus.
"Hex File parsing failure. Unknown record type."
I noted bellow description in ModusToolbox_IDE_User_Guide.pdf
You can use the HEX file with the Cypress Programmer tool to program the device.
Make sure you set the Reset Chip flag.
Refer to the Cypress Programmer 2.0 GUI User Guide for more information.
and I want to know how to set Reset Chip flag,
and does it relate with Hex File parsing failure.
Best regards,
Show LessHello,
I'm trying to get the BlinkyLED example to run on a PSoC6 BLE Pioneer Kit. The KitProg is updated to KitProg3 version 1.01.158.
I used the QuickPanel to debug the example and everything seems fine first. When eclipse switches to debug mode however, the program is not halted. In the Debug tab it reads Thread #1 (Running : UserRequest). The LED is not blinking (I guess LED5 should be). When I pause the application, I get the following errors:
Info : SWD DPIDR 0x6ba02477
Error: Failed to read memory at 0xfffff000
Info : SWD DPIDR 0x6ba02477
Error: Failed to read memory at 0xfffff000
Info : SWD DPIDR 0x6ba02477
Error: Failed to read memory at 0xfffff000
Info : SWD DPIDR 0x6ba02477
Error: Failed to read memory at 0xfffff000
I have tried with two boards, both show the same behavior. I also tried to use the Program launch option to see if the file was flashed correctly but still no blinking LED even after a power cycle.
Did I miss some important step or something?
Cheers
Michael
I am getting am error when programming a CY8CKIT-062-BLE with ModusToolbox which is preventing the device to be loaded.
This is the error that is seen:
** psoc6.cpu.cm4: Ran after reset and before halt...
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x00000f48 msp: 0x08047800, semihosting
Info : SWD DPIDR 0x6ba02477
Error: Failed to read memory at 0x00000000
Error: Unable to read IPC Lock Status register
Error: ROW @10000000 not erased!
target halted due to debug-request, current mode: Thread
xPSR: 0x21000000 pc: 0x00001f2c msp: 0x08047798
Error: failed erasing sectors 0 to 13
Error: flash_erase returned -4
Info : dropped 'gdb' connection
This was just working without issue but then started to show this error and I can no longer load code to the board. I've tried rebooting my PC and disconnecting the board and nothing seems to clear this.
Is there a way to reset the board to clear this?
- Jon
Show LessHello Cypress,
Fantastic news to see the new ModusToolbox is now available, and not just that, but also on Mac and Linux! Huge hoorays from those of us out here who don't run Windows on a daily basis.
Now, for me to fully move over to ModusToolbox, I need support for older PSoC chips as well. Will ModusToolbox be updated to support the PSoC 3/4/5 lines, or is it going to be PSoC 6+ only?
Thanks,
Joan
Show LessHi,
PSoc creator can export generated code as CMSIS pack,
and this pack can be used BY KEIL,
so I want to confirm whether Modus can export generated code as CMSIS pack too?
would you like to tell me method if it can support.
Best Regards,
Show LessHi!
This morning I downloaded and installed the ModusToolbox_1.0.0.2953-windows-install.exe.
Then I watched the four tutorial videos.
They were very nice and clear to be understood.
And I misunderstood myself ready to go.
I Started ~\ModusToolbox_1.0\eclipse\ModusToolbox.exe
I selected the menu File > New > ModusToolbox IDE Applicaiton
I selected Dev/Eval Kit
And selected CY8CKIT-062-BLE, as it's the only PSoC 6 evb I have right now.
For the Starter Application, although I wanted try some FreeRTOS,
I decided not to take chance, so I selected BlinkyLED.
When I selected "Finish" button, I got following dialog saying "Problem Occurred."
Although I'm sure that I'm good at encountering problem(s),
I'm a little bit bewildered about what to do next.
moto
Show LessI have downloaded and installed ModusToolBox, and would like to try it out.
I purchased the Cy8CPROTO-063-BLE and want to download the CE216795 project to it. I have downloaded the project.
I believe it will need to be modified, because I read somewhere pin numbers are different from PSoC 6 BLE Pioneer Kit (and possibly cpu).
I got down to Page 1, Operation in the pdf file. It indicated I should see KBA225201. I clicked on the link. On the Web Page, I get an error message:
Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.
I do not know email for the uploader of the project (which I won't spell out, but is J.T.) so I am contacting you here.
I am logged into the Cypress system. I am registered as an early adopter. I brushed my teeth this morning. <grin>
Questions:
1) How would I create custom components with ModusToolbox?
(i.e. use UDB to create AND-OR-XOR combinatorial logic) Please point me to some literature.
2) I have been able to narrow down the CY8CPROTO PSOC 63 to either CY8C6347BZI-BLD33 (without crypto) or CY8C6347BZI-BLD53 with crypto. Unfortunately, the specs on
the CYBLE-416045-02 module DO NOT specify the PSOC 63 being used by part number. The documentation on the CY8CPROTO-063-BLE does not specify the PSOC63 being used in the descriptive text, or the BLE module. I zoomed into a module photo and cross referenced the package and the BLE PSOC to come up with this possibility. I will now proceed to the next step.
**Update** I found the target MCU as CYBLE-416045-02 in the Choose Target MCU portion of the IDE application creation. Please specify this in your documentation in future revisions.
3) Do you need help translating C# to Qt? (For, e.g., your schematic designer). I work cheap.
Message was edited by: Wade Maxfield
Show LessHello,
I tried to program my KitProg (PSoC® 6 Wifi-BT) using the PioneerKitApp, and I get a message:
Error: *********************************************************************************************
Error: * KitProg firmware is out of date, please update to the latest version using fw-loader tool *
Error: *********************************************************************************************
Error: No Valid JTAG Interface Configured.
Where do I find the fw-loader tool and latest firmware?
Enrico
Show Less