Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

KeTa_1341526
Level 5
Level 5
10 likes received 5 likes given First like given

Hello,

Can I get the Wi-Fi Certification Test by developing with Modus?

Q1.

"RELEASE.md" of [Wi-Fi Host Driver (WHD) v1.91.2] had the following description.

[Includes WFA pre-certification support for 802.11n and WPA3]

In other words, does this mean that you are pre-certifying 802.11n and WPA3 (including WPA2) and pass the production test?

Also, does this Pre-Cert pass the test with Client and SostAP using WPA3 if it is CYW43012 described in "RELEASE.md"?

Q2.

Does the Modus environment provide a library such as WTS (Wi-Fi Test Suite) provided by WFA?

If No, how should the Certification Test be done?

Q3.

Does Modus support Wi-Fi Direct?

If yes, is it compatible with GO?

Also, has the environment passed the Wi-Fi Certification Test (including Pre Certification)?

Thanks

1 Solution
MuraliR_36
Moderator
Moderator
Moderator
250 sign-ins 250 replies posted 100 solutions authored

Hello

I apologize for the delayed response.

The support for WiFI direct on modus can be added.

The applications and Certification for WiFi on modus are under development and is planned to be released in the future.

Please contact your nearest Cypress/Infineon sales for further support.

Thanks

View solution in original post

0 Likes
1 Reply
MuraliR_36
Moderator
Moderator
Moderator
250 sign-ins 250 replies posted 100 solutions authored

Hello

I apologize for the delayed response.

The support for WiFI direct on modus can be added.

The applications and Certification for WiFi on modus are under development and is planned to be released in the future.

Please contact your nearest Cypress/Infineon sales for further support.

Thanks

0 Likes