Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ModusToolbox™ General Forum Discussions

Arha_4247766
Level 1
Level 1

Hi

Please help me with this

I Just installed ModusToolbox on Ubuntu 18 (ModusToolbox Version:  2.2.0 [Build ID: 2181])

1) Initially, I got this below error .

"Unable to find tools information: Cannot run program "/home/aravind/ModusToolbox/tools_2.2/modus-shell/modus-shell/bin/make" (in directory "/home/aravind/ModusToolbox/tools_2.2/modus-shell/make"): error=2, No such file or directory.

Is the CY_TOOLS_PATH set correctly?"

2)  I pointed the path to "/home/aravind/ModusToolbox/tools_2.2"  in 'Window--> Preference--> common tool location '

Then it could not find the modus-shell as below when i tried to open an example project

"Failed to locate modus-shell in /home/aravind/ModusToolbox/tools_2.2.'

3) Then I included modus-shell in the path in the common tool location as below . Now it does not even find project creator startup

"Unable to detect Project Creator startup after 10000 ms.

If this problem continues, try starting Project Creator stand-alone, then import the project using ModusToolbox import."

Screenshot from 2020-12-24 16-16-24.png

0 Likes
1 Solution
Arha_4247766
Level 1
Level 1

My bad .... I had not installed it properly.

Please ignore !!!

View solution in original post

0 Likes
1 Reply
Arha_4247766
Level 1
Level 1

My bad .... I had not installed it properly.

Please ignore !!!

0 Likes