Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ModusToolbox™ General Forum Discussions

rrusak
Level 1
Level 1
First like given First reply posted First question asked

Hello 

When I try to create a new project with Project Creator I get an error getting device_db:
mtb_err.jpg

Loading the device db
git: '9570/.modustoolbox/cache/git/https___github.com_Infineon_device-db' is not a git command. See 'git --help'.

INFO:Using the executable path for the tools directory.

ERROR:there was an error retreiving the asset 'https://github.com/Infineon/device-db' commit 'release-v4.1.0' - git: '9570/.modustoolbox/cache/git/https___github.com_Infineon_device-db' is not a git command. See 'git --help'.

ERROR:Global asset download of device-db loading completed with error.

ERROR:The asyncStepComplete failed for LoadFlag DEVICE_DB.

What could be the issue? I also noticed that the path to the cache starts with '9570/' although my user profile name is  'XPS 9570/', is there a problem with a space in the profile name? Thanks in advance for help.

Windows 10

Eclipse IDE for ModusToolbox™

Version: 3.0.0
Eclipse Build ID: 2749

 

0 Likes
1 Solution
MYKZ
Employee
Employee
10 replies posted 10 sign-ins 5 sign-ins

Please check if you have done everything as described in the https://www.infineon.com/dgdl/Infineon-ModusToolbox_3_0_Installation_Guide-GettingStarted-v01_00-EN....

section 6 Installing with spaces in user home directory

There is quite a few system variables you need to get setup.

View solution in original post

0 Likes
4 Replies
LeoMathews
Moderator
Moderator
Moderator
100 sign-ins 25 solutions authored 100 replies posted

Hi @rrusak 

Yes, a space in the user profile name path will cause this issue. In your case, the default path for device-db contains a space, which is why ModusToolbox cannot retrieve the asset.

If you have installed ModusToolbox in a custom location then please add the environment variable   CY_GETLIBS_GLOBAL_PATH = ~/.modustoolbox/global and restart ModusToolbox. Where the .modustoolbox folder will be in the same directory where ModusToolbox was installed in your system.

Thanks and Regards,
Leo

Thanks, and I also need to specify CY_GETLIBS_CACHE_PATH variable, but anyway it is working now.

But, unfortunately, I had one more following problem, when I try to create a project, there are errors in getting the project from the git.

Summary:

BSP: CY8CPROTO-063-BLE

Template Application(s): BMI160 Motion Sensor over I2C FreeRTOS

Application(s) Root Path: C:/main/workspace/code/mtw

Press "Create" to create the selected application(s).

Collecting application data...

Info: The following entered on the command line will create the exact same project as that created with the GUI tool:

C:/Infineon/Tools/ModusToolbox/tools_3.0/project-creator/project-creator-cli.exe --board-id CY8CPROTO-063-BLE --board-uri https://github.com/cypresssemiconductorco/TARGET_CY8CPROTO-063-BLE --board-commit latest-v4.X --app-id mtb-example-psoc6-bmi160-motion-sensor-freertos --app-uri https://github.com/Infineon/mtb-example-psoc6-bmi160-motion-sensor-freertos --app-commit latest-v2.X --cypress-tools C:/Infineon/Tools/ModusToolbox/tools_3.0 --target-dir C:/main/workspace/code/mtw --user-app-name BMI160_Motion_Sensor_over_I2C_FreeRTOS --use-modus-shell

Starting application creation for 'C:/main/workspace/code/mtw/BMI160_Motion_Sensor_over_I2C_FreeRTOS'.

Acquiring the application source 'https://github.com/Infineon/mtb-example-psoc6-bmi160-motion-sensor-freertos'.

usage: git remote add [<options>] <name> <url>

-f, --fetch fetch the remote branches

--tags import all tags and associated objects when fetching

or do not fetch any tag at all (--no-tags)

-t, --track <branch> branch(es) to track

-m, --master <branch>

master branch

--mirror[=(push|fetch)]

set up remote as a mirror to push to or fetch from

Application acquisition failed.

ERROR:Application creation failed.

ERROR:there was an error retreiving the asset 'https://github.com/Infineon/mtb-example-psoc6-bmi160-motion-sensor-freertos' commit 'latest-v2.X' - usage: git remote add [<options>] <name> <url>

ERROR: -f, --fetch fetch the remote branches

ERROR: --tags import all tags and associated objects when fetching

ERROR: or do not fetch any tag at all (--no-tags)

ERROR: -t, --track <branch> branch(es) to track

ERROR: -m, --master <branch>

ERROR: master branch

ERROR: --mirror[=(push|fetch)]

ERROR: set up remote as a mirror to push to or fetch from

ERROR:error cloning git asset 'https://github.com/Infineon/mtb-example-psoc6-bmi160-motion-sensor-freertos'-usage: git remote add [<options>] <name> <url>

ERROR: -f, --fetch fetch the remote branches

ERROR: --tags import all tags and associated objects when fetching

ERROR: or do not fetch any tag at all (--no-tags)

ERROR: -t, --track <branch> branch(es) to track

ERROR: -m, --master <branch>

ERROR: master branch

ERROR: --mirror[=(push|fetch)]

ERROR: set up remote as a mirror to push to or fetch from

Skipping export of the "BMI160_Motion_Sensor_over_I2C_FreeRTOS" application to Eclipse IDE for ModusToolbox™.

19 error(s), 0 warning(s)

Summary:

ERROR:Failed to create and export "BMI160_Motion_Sensor_over_I2C_FreeRTOS" application.


But when  I manually pull this commit(git clone --depth 1 --branch latest-v2.X https://github.com/Infineon/mtb-example-psoc6-bmi160-motion-sensor-freertos) everything works fine, what could be the issue?

Screen with error log in ModusToolBox IDE is below:

mtb_err2.png

0 Likes
MYKZ
Employee
Employee
10 replies posted 10 sign-ins 5 sign-ins

Please check if you have done everything as described in the https://www.infineon.com/dgdl/Infineon-ModusToolbox_3_0_Installation_Guide-GettingStarted-v01_00-EN....

section 6 Installing with spaces in user home directory

There is quite a few system variables you need to get setup.

0 Likes
rrusak
Level 1
Level 1
First like given First reply posted First question asked

Thank you for pointing out! I I followed the instructions in the sixth section and now everything works.

0 Likes
This widget could not be displayed.