Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ModusToolbox™ General Forum Discussions

Panometric
Level 5
10 solutions authored First comment on KBA First comment on blog
Level 5

We have been using the MTB flow to add driver libraries from vendors and OSS. This uses MTB make getlibs and git to bring the code in, with a version,  which is elegant. 

However, there is usually a case where you want to have a *.h file to customize the MTB, for example to redefine printf or malloc, or set some constants.   But the MTB start.mk file seems to work against us.  It prioritizes the mtb-shared version of the *.h file, rather than the project specific copy.  We can only make it work by deleting the mtb-shared version of the *.h, which is inelegant since these might be public repos.  

How can we force the MTB flow to prioritize our includes, over those in the mtb-shared directories  that are next to the *.c files being compiled? I expected that putting our dirs in makefile INCLUDES would do that, but they end up being last, not first. 

0 Likes
1 Solution
RodolfoGL
Employee
250 sign-ins 5 comments on KBA First comment on KBA
Employee

You can use the directive CYIGNORE= in the makefile to add a path that you want the compiler to ignore.

View solution in original post

0 Likes
3 Replies
RodolfoGL
Employee
250 sign-ins 5 comments on KBA First comment on KBA
Employee

You can use the directive CYIGNORE= in the makefile to add a path that you want the compiler to ignore.

0 Likes
Panometric
Level 5
10 solutions authored First comment on KBA First comment on blog
Level 5

@RodolfoGL How is this a solution? That will ignore the whole directory, not just one file that you need to override.  We need a way to change the search order to just prefer our code over the mtb code if it exists. 

0 Likes
RodolfoGL
Employee
250 sign-ins 5 comments on KBA First comment on KBA
Employee

You can ignore only the files you want to overwrite. Don't need to set the whole directory.

0 Likes