Hi!
This morning I downloaded and installed the ModusToolbox_1.0.0.2953-windows-install.exe.
Then I watched the four tutorial videos.
They were very nice and clear to be understood.
And I misunderstood myself ready to go.
I Started ~\ModusToolbox_1.0\eclipse\ModusToolbox.exe
I selected the menu File > New > ModusToolbox IDE Applicaiton
I selected Dev/Eval Kit
And selected CY8CKIT-062-BLE, as it's the only PSoC 6 evb I have right now.
For the Starter Application, although I wanted try some FreeRTOS,
I decided not to take chance, so I selected BlinkyLED.
When I selected "Finish" button, I got following dialog saying "Problem Occurred."
Although I'm sure that I'm good at encountering problem(s),
I'm a little bit bewildered about what to do next.
moto
Solved! Go to Solution.
Well, I'm afraid that I found the reason.
So I gave up the sample project and tried to create an empty project for CY8C6347BZI-BLD53.
Then I got following error dialog!
And now I understand the reason (or at least one reason),
that is in our company/office the security does not allow us run "bash"
So unless I can manage to convince the management/security
that I need to use bash and let them allow me to run one,
it will be very difficult to create a project...
moto
One thing I should have mentioned in the original post is that
I set my work space to
C:\Cypress\PSoC\PSoC6\MTW100
moto
I tried a few more times with different options, but all came back with similar errors.
Then I noticed that in the console pane it says
Log file(s) for this session are stored at: C:\Users\700650\AppData\Local\Temp\Logs2352646260215400188
So I went to dig that folder, attached is the log file I found there.
moto
Well, I'm afraid that I found the reason.
So I gave up the sample project and tried to create an empty project for CY8C6347BZI-BLD53.
Then I got following error dialog!
And now I understand the reason (or at least one reason),
that is in our company/office the security does not allow us run "bash"
So unless I can manage to convince the management/security
that I need to use bash and let them allow me to run one,
it will be very difficult to create a project...
moto
Hey Motoo,
I am so sorry you ran into all these problems. We do use bash as a shell to run commands like make. Your IT group probably does not want users running bash as a generic shell because it had security issues back in 2014 (See shellshock). The way we use bash would not be susceptible to that, and we use an old version that was prior to it having those vulnerabilities anyway. That Wikipedia page I reference even shows commands you can run to show it's not vulnerable. I think it is only a problem with Linux/Unix/Mac systems.
My belief is that if you removed /bin/bash (since your security team won't let you run it anyway), then it would find the bash in $CYSDK/tools. Check with your IT/security team to make sure it's OK by them.
Here is more about shellshock from Symantec.
Unfortunately, ModusToolbox (nor almost any tool) cannot run without a shell to execute commands, and the shell we use is bash.
Let us know how it goes.
Regards,
--Matt
Dear Matt-san,
Thank you very much for your information!
I was not quite aware of that bash bug.
Anyway, I asked my manager to submit bash usage permission application to the security.
Although I could not use bash whole day yesterday, this morning when I tried to start my cygwin, which has been dead quite a while now, the shell prompt came up just like the yesteryear.
Then I started ModusToolbox and tried to create an empty Modus IDE project for CY8C6347BZI-BLD53.
Yes, it worked fine this time.
Finally, I'm ready to start exploring the new territory.
Scotty, beam me up!
moto
P.S. A couple of additional notes
(1) I'm using "Windows7" not linux nor MacOSX
(2) Since the "Error Occurred" dialog does not have scroll bar
nor it saves the message (at least I know of),
unless I tried with an empty project,
I could not have found that the root cause was "bash"
Great, Tanaka-san! I am so happy you got past that.
With regards to the error message. You've uncovered something we had not anticipated. I'll talk to the developers about coming up with a better error message (or at least why it didn't get written to the log file).
Have you had a chance to look at any of the links/videos the Welcome page. I'd like to get some feedback on them and on our Quick Start Guide.
One thing i'd also like to point out is the Documentation. It's one of my favorite things. You get to it by going to Help->General Documentation like this
Best Regards,
--Matt
Dear Matt-san,
Thank you very much for your response and information!
> Have you had a chance to look at any of the links/videos the Welcome page.
> I'd like to get some feedback on them and on our Quick Start Guide.
I have watched the first 4 Video Tutorials, which made me feel like I'd like to try by myself.
Well, I'll check the "Quick Start Guide"
> One thing i'd also like to point out is the Documentation. It's one of my favorite things.
> You get to it by going to Help->General Documentation like this
I'll check that menu, too.
Again, thank you very much for your help(s)!
Best Regards,
19-Dec-2018
Motoo Tanaka
Dear Matt-san,
Following is my first trial and personal review of the Quick Start Guide
(1) Initial Screen shows Welcome page.
May be mentioning it could avoid some surprise(s)
After dismissing the "Welcome" we arrive at the workbench.
(2) Page 3 (Step 2)
As I don't have CY8CKIT-062-WIFI-BLE, I selected CY8CKIT-062-BLE
(3) Step 5
after "focus on the <app-name>_mainapp project.
Specifying the real name, for example
In this example, "BlinkyLED_mainapp"
would be easier to understand.
(4) May be showing the upper-left half (1/4) of the workbench
could be easier to locate/notice the project name.
(5) Add/Modify Application Code
The appearance of main.c when started first is totally different.
May be suggesting "scroll down the window up to where we see the code"
or something will be helpful for the "hardcore beginners"
(6) The Save/Save As commands will also available to select.
(May be I'm too picky but) I wonder if we should mention that
they are in the File Menu and/or in the menu icon bar.
BTW, Isn't "Save As" command always available?
(7) Configure Device Resource
The screen shot shows different project name "CapSenseSlider_config"
I would suggest to stick with the same project.
(8) Expand the <app-name>_config project
and double click the design.modus file.
It would be nicer to specify that you need to look into Quick Panel.
So I would say something like
Expand BlinkyLED_mainapp in the Quick Panel
then double click Configure Device
(9) When I double clicked the Configure Device,
Device Configurator Dialog showed up
and I received an Error Dialog.
Since I'm not sure if I should proceed, I'm stopped here.
(If I hack through, I won't be able to review the rest of the document)
moto
Well I noticed that if I only single click the "Configure Device" I could start Device Configurator without problem.
(It would be nice if Quick Panel detects "double click" and gracefully ignores the second click.)
moto
(10) Build the Application
"You can also select select Build ModusToolBox Application from the Project menu."
(10.1) there are two "select"s
(10.2) The Project Menu seems different
-> I needed to select "BlinkyLED_mainapp" in the Project Explorer then menu seemed similar, I miss the "set as active" menu.
Note: I build with Quick Panel "Build BlinkyLED Application"
(11) Program
The last message of program "shutdown command invoked" sounds
somewhat intimidating. Showing the image of display may mitigate it.
(12) After program flashed, my "CY8CKIT-062-BLE" did not blink any LEDs.
Note: May be there is/are problem with CY8CKIT-062-BLE sample...
(13) Debug the Program
I selected "BlinkyLED Debug (KitProg3)
And got following screen
And when I pushed the pause icon
So I suppose that if I did not have problem in the BlinkyLED project
I should have been able to build the project and invoke the debugger.
I will try to see if I can fix the project but anyway, it's not the topic of this thread.
moto
Tanaka-san,
Thank you for the detailed review and suggestions for our quick start. If you ever get tired of embedded design you should be a technical editor!
Now, let's talk about the BlinkyLED project issues. I have that same board, and it's working OK for me. I'm going to put aside the error messages for the debugger for the time being. Here are four things I would like you to do.
1. Do you see SW5 in the middle of that board? It's that white 3-position switch. Put it in the middle position so it will be configured like my board.
2. Can you give me the result of a fw-loader.exe command? Here's how to do that
i. Go to $CYSDK.tools\fw-loader-1.0\bin in Windows Explorer
ii. In the right pane, do a Shift-Right Click of your mouse and select "Open command window here"
iii. type fw-loader-1.0 --device-list
It should look something like
If it says "HID" instead of "BULK" that's OK.
3. In the Quick Panel, do a "Clean BlinkyLED Application" then Make, then just a plain Program (should be the bottom entry in the Launches section of the Quick Panel"
4. Look on the back of your board, bottom left-hand side, and tell me your revision number (for example Rev 11 or Rev 13)
We'll go from there.
Thanks,
--Matt
Dear Matt-san,
Following the observations
> 1. Do you see SW5 in the middle of that board? It's that white 3-position switch.
> Put it in the middle position so it will be configured like my board.
SW5 of my board was also in the middle position.
> 2. Can you give me the result of a fw-loader.exe command?
> 3. In the Quick Panel, do a "Clean BlinkyLED Application" then Make,
> then just a plain Program (should be the bottom entry in the Launches section of the Quick Panel"
(3.1) Clean selected and finished cleaning
(3.2) Build selected and built
(3.3) BlinkyLED Program (KitProg3) selsected
(3.4) Program finished
Note: At this point not LED blinking and even with RST switch pushed no blinking
(3.5) I also tried "BlinkyLED Debug (KitProg3)
(3.6) Debugger started (?)
> 4. Look on the back of your board, bottom left-hand side,
> and tell me your revision number (for example Rev 11 or Rev 13)
==============
121-60367-01 Rev 11
1744SO00652
==============
FYI, With PSoC Creator 4.2, attached project can be built, programmed, and debugged fine.
RED LED blinks ok. So I think that at least "some" part of the board is alive.
moto
moto-san, you need a new board. I know it may not seem like it since it
works with Creator, but I am pretty sure that is the issue.
Can you email me at mdl@cypress.com please?
Sorry for these issues.
--Matt
Dear Matt-san,
I have sent you a short mail.
Best Regards,
20-Dec-2018
Motoo Tanaka
I'm seeing the same issue with a Rev. 8 Board. I can program this board without issue with PSoC Creator but the BlinkyLED example from ModusToolbox does not work as the OP has shown. Does this mean I need a new board as well?
Jon, I am 90% sure yes.
I think it will still work fine with your current version of Creator/Programmer, but not ModusToolbox.
Who did you get the kit from? Can you ask them to send you a new one and Cc me (mdl@cypress.com)
on the communication?
We need a smooth way of doing this, but I don't think we'll be able to get anything set up before
the new year.
--Matt
I got the board from element14 but it is working fine with PSoC Creator so I am okay with that for now.
However, I am curious to know what version of PDL that ModusToolbox is using. I noticed when I tried to use PDL 3.1 with the CY8CKIT-062-BLE I had seen similar behavior where the code would compile and load without issue but would not run on the kit. I had to down rev to PDL 3.0.4 or earlier to get it to work so It would be interesting to know if there is a similar issue with ModusToolbox.
Hey Jon,
90% sure it's 3.1 in ModusToolbox.
--Matt
Then I am 99.99999% sure there in lies the issue.
If there is an option in ModusToolbox to down rev the PDL to say 3.0.4 then I would suspect it would work with the older BLE Pioneer kit.
Jon
Unfortunately, I don't think there is a way. I believe when you update an SDK in ModusToolbox,
you get the whole $CYSDK/libraries/psoc6sw-[version] directory. There is no separate PDL unit.
I could be wrong about that. There are folks working on this. Maybe there will be a solution that
doesn't involve replacing the kit.
--Matt
There is a PDL folder under:
ModusToolbox_1.0\libraries\psoc6sw-1.0\components\psoc6pdl
Jon
Hi,
Last night (in Japan) in the following thread
CY8CKIT-062-BLE Setup Only requires PDL 3.0.1
msur-san uploaded attached startup file.
When I backed up and replaced startup_psoc6_01_cm0plus.S at
C:\Users\<MyUserName>\ModusToolbox_1.0\libraries\psoc6sw-1.0\components\psoc6pdl\devices\psoc6\startup\gcc
I could finally build and debug BlinkyLED with my CY8CKIT-062-BLE (Rev 11) via ModusToolbox!
Thanks msur-san!
moto
Moto,
Yep, and no need to have the board replaced. I'm still recovering my environment and plan to confirm this as well as soon as I have Modus up and running again. The adjusted startup script does work with PSoC Creator 4.2 and PDL 3.1.0 and though.
Cheers,
Jon
Dear Jon-san,
> The adjusted startup script does work with PSoC Creator 4.2 and PDL 3.1.0 and though.
Thanks!
So we are now OK with cm0p side of startup.
I wonder if similar issue(s) may arise with the cm4 side,
we will find it along the way we explore more about ModusToolbox.
And meantime, I wonder if the startup with Cy_SaveIRQ and Cy_RestoreIRQ bothers the newer boards (Rev 13~).
Best Regards,
27-Dec-2018
Motoo Tanaka
I have just run diff on
PDL3.0.4 startup_psoc63_cm4.S
and
PDL3.1.0 startup_psoc6_01_cm4.S
and there surely was the same difference
=====================
269,289d276
< /* Saves and disables the interrupts */
< .global Cy_SaveIRQ
< .func Cy_SaveIRQ, Cy_SaveIRQ
< .type Cy_SaveIRQ, %function
< Cy_SaveIRQ:
< mrs r0, PRIMASK
< cpsid i
< bx lr
< .size Cy_SaveIRQ, . - Cy_SaveIRQ
< .endfunc
<
< /* Restores the interrupts */
< .global Cy_RestoreIRQ
< .func Cy_RestoreIRQ, Cy_RestoreIRQ
< .type Cy_RestoreIRQ, %function
< Cy_RestoreIRQ:
< msr PRIMASK, r0
< bx lr
< .size Cy_RestoreIRQ, . - Cy_RestoreIRQ
< .endfunc
=====================
So we may be able to hack the startup for cm4, too
or may be we'd better wait for Cypress's "official" fixed version.
moto
I have just confirmed that with the startup file,
I also could program and debug BlinkyLED on my colleague's
CY8CKIT-063-BLE (Rev 😎
moto
Moto/Jon,
It is not required to update the M4's startup file. The functions are used by boot code, which executes in M0+. So no need to update/change M4 startup files.
Regards,
Meenakshi Sundaram R
Meenakshi and Moto-san,
I can confirm that I was able to load and run the BlinkyLED ModusToolbox Example with my rev. 8 PSoC 6 BLE Pioneer Kit using the changes to the M0+ startup file.
Since there appears to be multiple versions of the PSoC 6 BLE Pioneer Kit, perhaps it would be best to put some sort of check in the startup file to accommodate the differences between boards; that is if it is possible.
Is there a ModusToolbox and/or PDL GitHub repository that this will be pushed to once it is signed off?
Jon,
It will be a ModusToolbox SDK release, if we decide to add those functions. It should be noted that the "Cy_SaveIRQ" and "Cy_RestoreIRQ" APIs are replaced with Enter/ExitCriticalSection APIs in the newer version (which makes sense). Somehow the *A flash boot seem to use fixed Address for the Save/RestoreIRQ calls. Anyway our SW team is out on holiday and will get back with proper answer when they get back on the defect ticket I raised.
Regards,
Meenakshi Sundaram R
And yeah to add to my previous response - the modified startup should work for newer version kits as well (I have tested ). In fact, the startup does not impact any functionality for the newer version. It possibly may have unused code (Cy_SaveIRQ and Cy_RestoreIRQ) if not optimized out by compiler.