- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Dear Sirs and Madams,
Please tell us how to realize the following connection used in PSoC Creator with Modus Toolbox.
PSoC Creator will automatically wire normally.
We would like to realize it with PSoC4S MAX.
I did the following procedure for Modus Toolbox, but it cannot be set correctly.
(1) Start Device Configurator3.1
(2) Enable CTBm 0 and SAR ADC 0 from Peripheral Tab
(3) Set CTBm0 to follower
(4) Set Input of CTBm0 to P1[0:7], set output of CTBm0 to "SAR ADC 0 vplus"
(5) Set "number of channels" to "1" and Ch0 Vplus of SAR ADC to "CTB 0 OpAmp 0 out_1x"
Setting of CTBm 0
Settings of SAR ADC
Analog-Routing
When I run the build, I get an error and cannot analog-routing properly.
Please let us know if there is a problem with my settings, Or is it possible to get a sample project?
Regards,
- Labels:
-
ModusToolbox General


- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @MaMi_1205306,
I am attaching a PSoC 6 project for muxing the inputs at OpAmp ( configured as a follower).
>> P9[0] is configured as the input to the opamp.
P9[0] is connected to the AMUXBUS A. P9[1], P9[2] and P9[4] are connected to P9[0] using AMUXBUSA in a cycle.
You can refer to the project and develop your own project.
>> You can refer to the PSoC 6 PDL for further configuration.
Please, let us know if you need further clarification.
Thank you
Best Regards
Raj Chaudhari

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Raj-san,
Thank you for your support.
I imported and confirmed for your attached project.
However, Device configurator 3.10 cannot be opened.
In the first place, I cannot be confirmed for the analog routing because "Device configurator" is no choice in the tool.
So I tried to set it with PSoC4S MAX, but "AMUXBUS A" is not displayed at the pin connection destination.
Does "AMUXBUS A" in your comment refer to "MSC 0 amuxbus_a" or "MSC 1 amuxbus_a"?
I also don't understand that We can't select "PASS_amuxbus_a/b".
Regards,