- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Is there a way to create and configure project for a specific Target PN without starting from a dev kit template in ModusToolbox 2.0? We have a schematic design and need to move beyond the PNs associated with dev kit templates i.e. the PSoC6 PN we are using is not provided in a kit template.
Thank you,
Wess
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Wess,
You can choose a kit template that has the part number which is of the same family as the one you want. Once the project is created, you can click on Device Configurator. Once the configurator window opens, use File > New.
Here you can create a new "design.modus" file targeting the MCU device PN you want and save it in the default location by overwriting the existing one.
Inside the "libs\TARGET_<BOARD_NAME>\COMPONENT_BSP_DESIGN_MODUS\" directory, delete the GeneratedSource directory. Also, delete the files "design.cycapsense" and "design.cyqspi" if you don't need CapSense and QSPI.
Make necessary changes in the device configurator based on your application and build your application.
You can also refer to the section "Create your own Board Support Package" in BSP User Guide as shown below to create your own BSP package:
Regards,
Dheeraj