Hello Team,
I am trying to program CYBT-343026-01 module using external FTDI (FT232RL USB to TTL) using MODUS toolbox. I have done following connection.
FTDI CYBT module
+3.3V + 3.3V
Gnd -Gnd
Txd -Rxd
Rxd -Txd
RTS -CTS
CTS -RTS
On MODUS toolbox console shows ERROR: unable to find CMSIS-DAP Device.
how to solve this error kindly let me know.
Thanks & Regards,
Akshay
Solved! Go to Solution.
Hi @Akshay_C ,
Firstly, we recommend you to upgrade to the latest MTB version, ie MTB 2.3 for your application.
https://www.cypress.com/products/modustoolbox
Since you are using a USB-UART bridge, we will be using the HCI UART for programming. Therefore, you need to use the Program option and not the Attach_Kitprog3_Miniprog4 which is used for openOCD attaching to running target without initial programming.
Please let us know if this resolves the issue.
Hi @Akshay_C ,
Can you ensure that you have followed the connections between the USB-UART device and the CYBT module are provided in the CYBT-343026 eval board?
https://community.cypress.com/t5/ModusToolbox-General/CYBT-343026-Module-Programming/td-p/279896
Can you share the screenshot error log you see from the Modustoolbox?
Please let us know which version of Modustoolbox you are using.
Hi @BragadeeshV
Yes I have done same connection as provided in CYBT-343026 eval board schematic.
Kindly check below connections.
I am using ModusToolbox IDE v2.0 & Getting Below Error log.
Regards,
Akshay
Hi @Akshay_C ,
Firstly, we recommend you to upgrade to the latest MTB version, ie MTB 2.3 for your application.
https://www.cypress.com/products/modustoolbox
Since you are using a USB-UART bridge, we will be using the HCI UART for programming. Therefore, you need to use the Program option and not the Attach_Kitprog3_Miniprog4 which is used for openOCD attaching to running target without initial programming.
Please let us know if this resolves the issue.