Announcements

Community will be in read-only mode on 25th Sep for 10 hours. Click here for more details

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Memories Forum Discussions

Browse the Community

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.

7267441 1609

Hyper Flash

The HyperFlash NOR Flash memories Forum offers discussions on automotive advanced driver assistance systems (ADAS), automotive instrument cluster, automotive infotainment systems, and communication equipment.

429634 100

Hyper RAM

HyperRAM™ memory Forum discusses self-refresh DRAM operating on the 12-pin HyperBus interface. With a read throughput up to 333 MB/s, the HyperRAM for SoCs with limited on-board RAM providing external scratch-pad memory for fast read and write operations.

369556 92

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.

1148832 468

SRAM

Discussion forum for SRAM related topics.

1017592 448
filter icon

Featured Discussions

Sort by:
MAO
Nor Flash

S25FL128SAGMFI000
Do you have experience with the above model numbers operating at clock frequencies below 300 kHz?

cyldz
Nor Flash
Hello, I am using S25FS512SAGNFI011 Nor Flash for the FPGA Arria 10 configuration. I generated .jic file from .sof file as described in the document A... Show More
MAO
SRAM

Please tell me about θjb or Ψjb of CY7C1041G30-10ZSXI made by Infineon as it was not mentioned in the datasheet.

Ankit26
Nor Flash
While attempting to flash data onto the memory, we have encountered persistent problems with memory corruption and functionality. Specifically, we hav... Show More
MAO
Nor Flash

Please tell me about θjc or Ψjt and θjb or Ψjb of Infineon S29AL016J70TFI010.

chris-
SRAM

Hello,

Do you know if there is SEE testing data available for the CY7C185 SRAM?

-Chris

rkm151
SRAM
Hello,   Can this memory be ordered as lot sorted for the standby current?  Can you provide the manufacturing distribution for the standby current? Show More
Amatw
Non Volatile RAM (F-RAM & NVSRAM)
Hello, I am looking for a software which writes data to FRAM (FM25V20A-G) from PC. Can FLASH USB Programmer New 8FX work for FRAM also? If it doesn't,... Show More
MAO
Nor Flash
PSCK/tCH/tCL are available as AC specifications for SCK duty ratio, and for tCH/tCL, Notes 30,Notes 30. ±10% duty cycle is supported for frequencies ≦... Show More
fz_ghazavi
Non Volatile RAM (F-RAM & NVSRAM)
I want to find a drop-in replacement for FM25L04B because it has errata in writing procedure, I changed it to FM25CL64B but it does not work. any advi... Show More
Category Information

Memories

Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.