Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Memories Forum Discussions

Browse the Community

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.

8975872 1696

Hyper Flash

The HyperFlash NOR Flash memories Forum offers discussions on automotive advanced driver assistance systems (ADAS), automotive instrument cluster, automotive infotainment systems, and communication equipment.

540303 109

Hyper RAM

HyperRAM™ memory Forum discusses self-refresh DRAM operating on the 12-pin HyperBus interface. With a read throughput up to 333 MB/s, the HyperRAM for SoCs with limited on-board RAM providing external scratch-pad memory for fast read and write operations.

485503 107

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.

1445327 501

SRAM

Discussion forum for SRAM related topics.

1246114 466
filter icon

Featured Discussions

Jakub_Bieryt
Non Volatile RAM (F-RAM & NVSRAM)
HelloWe are using FRAM CY15B104QI memory in our project. We are using MSP430FR5994 microcontroller and we want to communicate with FRAM using SPI.  We... Show More
Msalem000
Nor Flash
Could you please confirm the lifecycle status for this package "PQFP" in this series "S29CL032J" ? Show More
Pacaci
Nor Flash
Hello, I have custom-designed a PCB that incorporates an MCU board and a Nor Flash, specifically the S25FL512SAGMFMR10 part. Currently, I am developin... Show More
erfan
Non Volatile RAM (F-RAM & NVSRAM)
I am using CY14U256LA-BA35XI as replacement for STK12C68-L35M replacement. Not using A13 and A14 as only 64kbit is used. HSB not connected as only pow... Show More
19Ronny87
Hyper Flash
Guten Tag zusammen. Könnten Sie mir bitte mitteilen, ob es sich bei dem S29GL256S11DHVV20 auf dem Bild um ein Original handelt (Marking)? Wenn ja: Wir... Show More
kmishra93
Hyper RAM
Hi Team,     One of the project, I have interfaces hyperRAM S27KS0641DPBHI020 to croslink-NX FPGA. I have hyperram controller IP provided by infineon.... Show More
lukasfrank
Nor Flash
Hi Dear Authorized,   I am trying to use HyperFLASH over FlexSPI Interface over HyperBUS and some errors occured during test on my custom board which ... Show More
kmishra93
Hyper RAM
I have interfaced 64MB hyperRAM (S27KS0641DPBHI020) with FPGA on board.  I am using infineon controller, I have written master to handle hyperram slav... Show More
Translation_Bot
Non Volatile RAM (F-RAM & NVSRAM)
We used Infineon's IC (p/n: S25FL064LABMFV000) to enter QPI mode and it was locked and could not be unlocked.smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t... Show More
ToddBailey
Non Volatile RAM (F-RAM & NVSRAM)
Hi, Does Infineon / Cypress have radiation test data on FRAM CY15B104Q (full part number CY15B104Q-SXI or similar) or on this part family? Specificall... Show More
Category Information

Memories

Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.