- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Is there an example of SD card read / write using FAT32 somewhere?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Actually, after getting more familiarized with Mbed OS, it does support an SD interface with FAT file system, but, here is the catch: the current implementation only supports single line (MOSI/MISO) SPI interface to the SD card. In order to use the SDHC interface of PSoC 6 there are two possible routes:
a. Modify the SDBlockDevice class to use the HAL Interface to the SDHC instead of SPI, or...
b. Thanks to the layered design of Mbed OS, create a new BlockDevice derived class for SDHC using Cypress HAL library.
Any file system in Mbed OS can then use this peripheral interface class.
Option b. seems to be more logical approach and the route of less effort, I think. Working on it now...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Refer to this code example:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks Rodolfo, however that is not what I´m looking for. I want to implement an SD card file Read/Write using the CY8CPROTO-062-4343W prototyping kit. I will use the the FAT32 file system available in Mbed OS so the file can be later read in a PC or Mac system.
I guess I will have to start from scratch.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
If you are using mbed, you can refer to this one:
https://github.com/ARMmbed/mbed-os-example-filesystem
Both examples use a file system:
mbed: LittleFsSystem
ModusToolbox: FatFS
I'm not sure about the mbed, but the ModusToolbox one uses FAT32.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Adding to Rudolfo's comment, you can modify the filesystem used in the GitHub - ARMmbed/mbed-os-example-filesystem: The Mbed OS file system example from LittleFS to FatFS. Refer to the section "Changing the File System" in the Readme.md file in the repository for more information on how to do this.
Regards,
Dheeraj
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Actually, after getting more familiarized with Mbed OS, it does support an SD interface with FAT file system, but, here is the catch: the current implementation only supports single line (MOSI/MISO) SPI interface to the SD card. In order to use the SDHC interface of PSoC 6 there are two possible routes:
a. Modify the SDBlockDevice class to use the HAL Interface to the SDHC instead of SPI, or...
b. Thanks to the layered design of Mbed OS, create a new BlockDevice derived class for SDHC using Cypress HAL library.
Any file system in Mbed OS can then use this peripheral interface class.
Option b. seems to be more logical approach and the route of less effort, I think. Working on it now...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Glad to hear that you are able to move forward. Please do create a new thread if you face any issues during the implementation. Marking this one as resolved as it answers the original question of how to begin with SD card implementation in Mbed.
Regards,
Dheeraj