MOTIX™ MCU Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
In my project I want to apply the break with below FET status, will it be considered as break condition?
L1,H1,L2,H2 (Ch_en, Ch_off, Ch_en, Ch_off) because I observed back electromotive current when I used below option:
(Ch_On, Ch_off, Ch_On, Ch_off).
Reference board is TLE9869.
Show LessHi all
TLE9879_EvalKit_BLDC_HALL
The official program, adjust the motor speed using the potentiometer set Poti_Handler(), the motor can work normally. However, if you set a fixed speed, such as Emo_SetRefSpeed(1000) , then when the motor starts, it needs to be turned by hand to enable the motor to start normally, otherwise it will not turn.
I've tried to debug the startup duty cycle and the PID parameters, but nothing works.
I hope I can get help.
BEST REGARDS
Show Less大家好。
TLE9879开发板,官方自带程序,调节速度使用电位器设定,电机能够正常工作。但是如果设定一个固定转速,比如Emo_SetRefSpeed(1000 ),那么电机启动的时候,需要用手转一下,电机才能够正常启动运转,否则就不转动。
已经试着调试过启动占空比,给定的速度,以及PID参数,都不管用。
问下能够得到指点一下,感谢!
Show Less
1.TLE9879 _Evalkit_v1.4 What are the main functions of swdio R46 and swclk R50 and how are these values selected?
2.tle987x series power up swd part power up timing have a detailed explanation?
--------
Infineon-Z8F80032532_HW_Design_Guideline-ApplicationNotes
-----
Infineon-BLDC_shield-UserManual-v01_02-EN
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/SWD/td-p/716438
Show LessFor help, what does 148BB434 B,each number and letter in the red box mean?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/Nor-Flash/%E5%A6%82%E4%BD%95%E8%AF%BB%E5%8F%96%E8%8A%AF%E7%89%87%E4%B8%8A%E4%B8%9D%E5%8D%B0-%E4%B8%9D%E5%8D%B0%E5%86%85%E5%AE%B9%E5%8C%85%E5%90%AB-%E6%95%B0%E5%AD%97%E5%92%8C%E5%AD%97%E6%AF%8D%E5%88%86%E5%88%AB%E4%BB%A3%E8%A1%A8%E4%BB%80%E4%B9%88/td-p/715811
Show LessMOTIX ™ Motor Control Library FOC demo with TLE987x and LIN communication cannot extract pack. I reload the package, but it always fail.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/MOTIX-Motor-Control-Library-FOC-demo-with-TLE987x-and-LIN-communication-cannot/td-p/714414
Show LessI have performed the DC Link short to GND in order to test 7th MOSFET (reverse polarity MOSFET) turn OFF time during fault condition in BLDC application. In this test, the DC link is short to GND and ultimately VDH pin of TLE9877 short to GND. The turn OFF time of the Gate voltage of the 7th MOSFET and the charge pump is around 500us even if I remove all the Software delays.
My questions are:
1. Why do I have this delay even though I don't have any Software delay?
2. What is happening inside TLE9877, when VDH pin short to GND?
3. How could I reduce this 500us delay to Zero?
NOTE: The charge pump (VCP) under voltage diagnosis is enabled with low voltage threshold 7.325V and filter time 16us.