MOTIX™ MCU Forum Discussions
Hi, I am using REF_WATERPUMP100W board, so for that which debugger should I use. Can I use the J-LINK EDU MINI from Segger Microcontroller Systems. also please share the link for debugger if possible. Thank you
Show LessCurrent Issue: After attempting to flash codeflash (0x11000000-0x1100f000) during user code run, flash flashing fails and interrupts stop responding.
Is it possible to write codeflash directly, and if so, how should I do it?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/tle9877-%E7%9B%B4%E6%8E%A5%E5%88%B7%E5%86%99codeflash/td-p/476179
Show LessCurrent Issue: After changing the interrupt vector and app start address (0x11000000→0x11005000), the program cannot run to reset_handler.
Is this problem caused by the fact that the "bootrom can only jump to 0x11000000 "at the end of its run? If yes, how to change this jump address?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/tle9877-%E4%BF%AE%E6%94%B9bootrom%E8%BF%90%E8%A1%8C%E7%BB%93%E6%9D%9F%E5%90%8E%E8%B7%B3%E8%BD%AC%E5%9C%B0%E5%9D%80/td-p/475132
Show LessTLE9879QXA40 using pack 1.6.0 of DMA_UART example, open V2 configuration (version 2.7.3) reported an error, many parameters do not show up, see attachment!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/Wizard-config-%E6%8A%A5%E9%94%99/td-p/475053
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/TLE9879-sensorless-FOC-%E7%94%B5%E5%8E%8B%E7%8E%AF%E7%9A%84-kp-ki%E8%AE%A1%E7%AE%97%E6%96%B9%E6%B3%95/td-p/473670
Show Less大家好 :
关于ADC和DMA 有几个疑问,想得到帮助。
1.官方例程TLE9879_DMA_ADC1中,adc_ch_result[DMA_CH0_NoOfTrans]数组设置为8,但是IFXCONFIG里面,图1所示序列模式勾选了14个(7个通道+7个通道4重复采集),那么这个地方,DMA在传数的时候,是不是把前几个就给覆盖了?
2.DMA配置里,ADC1->RES_OUT7.reg这个配置是干嘛用的?
3.DMA完成中断触发条件是什么,是完成一个通道还是完成整个一次多通道扫描?
4.采集的数为什么设置为32位的,ADC是12位的。
5.如果我想测量2通道的ADC的数,一个P2.4的电压+一个VDH的电压,循环扫描,实时更新,该怎么配置。
因为资料较少,看了半天文档也是不明所以,希望得到解答。
Show Less
Hello All,
Need some help here.
I want to configure CAN based WAKE UP. However is there any provision in TLE9893 where I can filter/choose CAN Messages for selective WAKE UP.
In User Manual, there are two blocks mentioned as 'Wake receiver' and 'WUP detection' to generate WAKECAN. If there are details over these two blocks, it would be helpful.
Thanks and Best regards,
Nikhil
Show LessClicking on the download link on the official website ( Software overview - Infineon Developer Center ) shows an error, how can I download the demo program.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/%E5%A6%82%E4%BD%95%E4%B8%8B%E8%BD%BDBLDC-SHIELD-TLE9879%E7%9A%84demo%E7%A8%8B%E5%BA%8F/td-p/471016
Show Less