MOTIX™ MCU Forum Discussions
Hey team,
I bought TLE9879 eval kit from Infineon for our BLDC WIPER MOTOR application. I have some requirements from my side in our application.
1.EMI/EMC - SHOULD BE IN CLASS 5 - AS A MOTOR & IN VEHICLE.
2.NOISE – ENSURE SMOOTH RUNNING - (harmonic distortion should be reduce).
3.SPEED - DIFFERENCE BETWEEN LOW AND HIGH SPEED MUST BE IN 18 RPM.
4.PARKING POSITION – MUST BE IN ± 2° (expecting ± 1° for BLDC)
5.ENVIRONMENTAL TEST ASPECTS SATISFICATION – (salt, dust, vibration, waterspray, mud etc...)
These requirements are should be satisfied with the EVAL KIT with tuned programming? Could you help me in programming for the above requirements.?
Hope your answers satisfied our requirements.
Regards
pgm
Show Less采用keil例行程序,采用本公司的五极电机,可逐渐增加负载开环启动故障,如何调整开环负载增加
Dear Team,
We have implemented two analog reading at port 2.0 port 2.1 via sequencer. and one through ESM
now we required to take one more analog channel reading via sequencer at port 2.2, but once we do it disturb the LIN communication.
any suggestion or advice will be helpful.
Show LessHi,
In our application we are trying to send output signal in specific cases via LIN pin to the master. This output signal should be duty modulated PWM signal so we are not trying to communicate via LIN protocol.
I could not find how to send duty modulated PWM data via LIN pin on the board. Is there a way to do it ?
Show LessHi Team,
I am new to TLE controllers. I am trying to run a sensorless BLDC motor and reading the current feedback. I used the example code BLDC_BC_BEMF_EXAMPLE_TLE987X and I am able to run the BLDC motor properly using CCU6. While adding the configuration for reading the ADC1_CH1, my callback is getting called by the ADC value is not getting change with changing in the speed value. The ADC configuration is attached with name ADC1_CH1_config.
Also, while change the ccu6 configuration from edge_alligned mode to central-alligned mode, my motor is not running(to read the motor feedback properly in centre-alligned mode)
I am attaching the whole project here.
can somebody please have a look and help me here as I am stuck in this situation for sometime now.
Show Less
We plan to use a chip from the TLE987x family in development.
Is it possible to protect flash firmware from further reading (readout protect)?
In the documentation, I read that the chip is always available for any operations via SWD. Show Less
在调试面板上有 Clokwise 和 counter Clockwise的选项. 是否有脚本指令,可设置驱动电机反转?
Sir,
Kindly provide the algorithm/programming for circuit protection( over current, over voltage, over temperature, under voltage) of the TLE9879 eval kit.
This will useful to work for us with the eval kit which we procured from INFINEON.
Regards
pgm
Show Lesskeil version 5.37.0
Refresh Pack descriptions copy Check for updates Cannot install Pack Infineon.TLE9879QXA40_eSL-BAS-LIN-EVAL.1.3.5. Cannot extract Pack Check for updates
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/motix-lin-demo-pack%E8%A7%A3%E6%9E%90%E4%B8%8D%E4%BA%86/td-p/731462
Show LessDear Infineon Staff.
I have to develope an application which uses LIN interface. I would like to know if there is already an implemented stack I can use or if I have to develope it by myself.
If it were already available a stack, is it certified for LIN Compliance? If It were not certified can you suggest me required steps in order to get it certified?
Regards
Show Less