MOTIX™ MCU Forum Discussions
Dear Team,
Thank you for your kind support,
is there any way to do wake up MCU after VS is goes down to 3V , without POR (Hardware reset)?
Thank you in advanced!!
Show LessGreetings,
I am working with TLE9879 Eval kit with ARM Keil µvision5 software. I bought a application file from Infineon "TLE987x-eSL-BAS-LIN-EVAL" and working it with keil software.
I got the following error regarding compiler, kindly sort out this for my further proceedings with Eval kit.
In my exploration with this error, the programming file is not suitable for this free versioned software. Isn't it?
Show Less
Hi,
I would like to enable Can Rx interrupt in TLE 9893. I am basically looking for a callback function with the received/transmitted CAN bytes .!! I am looking into the config motix tool via keil IDE. So sure about the correct settings. Can you help me in this ..!!
Thanks
Prakash
Show Lesshttps://softwaretools.infineon.com/software?q=foc,DEMO code can't be downloaded.
Is there a downloadable link for this, please?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/TLE-987X/td-p/498254
Show LessHi All,
I would like to warn the community about a bug I believe exists in the WDT1 driver of the TLE987x SDK.
The variable WD_Counter must be defined as volatile. That is because each variable that is manipulated in an Interrupt Service Routine must be defined as volatile in order to prevent the compiler from optimizing it. The WD_Counter is incremented in SysTick_Handler.
I have discovered this bug when I have enabled the compiler optimizations. Then I noticed that the microcontroller has been reset regularly on the WDT1 defined period.
I'm a little bit disappointed that such a simple mistake exists in an official SDK, which perhaps is widely used. It also means that it is not sure how many similar mistakes exist in the other drivers.
Best Regards,
Tenko Yavashev
Show LessHey team,
I bought TLE9879 eval kit from Infineon for our BLDC WIPER MOTOR application. I have some requirements from my side in our application.
1.EMI/EMC - SHOULD BE IN CLASS 5 - AS A MOTOR & IN VEHICLE.
2.NOISE – ENSURE SMOOTH RUNNING - (harmonic distortion should be reduce).
3.SPEED - DIFFERENCE BETWEEN LOW AND HIGH SPEED MUST BE IN 18 RPM.
4.PARKING POSITION – MUST BE IN ± 2° (expecting ± 1° for BLDC)
5.ENVIRONMENTAL TEST ASPECTS SATISFICATION – (salt, dust, vibration, waterspray, mud etc...)
These requirements are should be satisfied with the EVAL KIT with tuned programming? Could you help me in programming for the above requirements.?
Hope your answers satisfied our requirements.
Regards
pgm
Show Less采用keil例行程序,采用本公司的五极电机,可逐渐增加负载开环启动故障,如何调整开环负载增加
Dear Team,
We have implemented two analog reading at port 2.0 port 2.1 via sequencer. and one through ESM
now we required to take one more analog channel reading via sequencer at port 2.2, but once we do it disturb the LIN communication.
any suggestion or advice will be helpful.
Show LessHi,
In our application we are trying to send output signal in specific cases via LIN pin to the master. This output signal should be duty modulated PWM signal so we are not trying to communicate via LIN protocol.
I could not find how to send duty modulated PWM data via LIN pin on the board. Is there a way to do it ?
Show Less