MOTIX™ MCU Forum Discussions
text.format{('custom.tabs.no.results')}
Resistance and capacitor selection, how to determine the configuration parameters, thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/TLE9879-EvalKit-V1-4-%E5%85%83%E4%BB%B6%E9%80%89%E5%9E%8B/td-p/632816
Show Lesstle987x evb, BSL Tool for MOTIX™ MCU can adjust firmware parameters and download firmware 2. Can it be debugged through USB or external swd?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/motix-%E5%B7%A5%E5%85%B7%E4%BD%BF%E7%94%A8/td-p/631003
Show LessDear all,
I'm trying to drive the motor with TLE9877QAX40. I've noticed that in this version of the software,
the relevant code in the document Micro Inspector Pro Getting started has been commented out.
So I want to make sure that Micro Inspector Pro still works.
Show LessHello,
I have a custom board using TLE9879 which copies the Evaluation board of TLE9879 for the Arduino.
The only difference is that my chip select pin is P0.0 (BOARD2) instead of P2.3 (BOARD1).
As a consequence, the blinky test program is stuck in a loop where BOARD1 cannot be initialized.
Can I change this behaviour in the Arduino library or do I have to adjust the default firmware?
Thank you very much in advance.
Best Regards,
Thai.
Show Less
Hi,
I am using NVM read /write function for storing the values in the internal flash of TLE9893 . Example : i am using user_nvm_page_write function from bootrom.h file. i dont have access to user_nvm_page_write() function in the bootrom.c files. Is that all the NVM functions are precompiled the service pack 1.0.0. It would be great it someone could help me in this .!!
Thanks
Prakash
Show LessProduct Battery cooling pump
Product Battery cooling pump
Please provide cheapest solution for Battery cooling pump
Please find requirements below
Fluid 50% ethylene glycol in water
Motor
Bldc motor 330 watts
0.7 nm torque
4800 rpm rated speed
Motor controller requirent
FOC or block
Applications on board requirement
Software to control the motor
Power requirement
24 v
Asil Level requirement
No asil
Automotive requirement
Yes
Show LessDear all,
I tried to independently control MOSFETs' on and off on of the three-phase bridge for TLE987x based on Demo"BLDC_SENSORLESS_FOC_EXAMPLE_TLE987X". For example, open the all low-sides and close the all high-sides. But actually Vgs of all low-sides keep 0v via OSC. Can you help me find a possible cause? Thank you in advance!
Show Less
Hi Infineon,
Is there anyone know how to control the motor speed by adjusting the duty cycle of PWM on PIN LIN?
Hi,
I want t0 use TLE9877QXA40 to run a motor demo. I downloaded the demo software from MOTIX™ TLE987x Motor Control FOC Demo - Infineon Developer Center
I see it's used for TLE9879, is the software universal? If not, what changes do I need to make.
Show LessKeil V5.36.0.0
Processor TLE9853QX
The computer used for development crashed. Keil and Configwizard were loaded on another PC.
The same version of Keil as on the original PC but files have different dates.
When comparing files I noticed that the ARMCC folder was not included in the latest instillation so I copied the folder from the original hard drive which resolved the above error.
Now I am getting the error: Fatal error: C3900U: Unrecognized option '-abdfrvy+glpsu'.
Can you please direct me on how to resolve.
Fatal error: C3900U: Unrecognized option '-abdfrvy+glpsu'.
Show Less