MOTIX™ MCU Forum Discussions
I have the BLDC motor shield with TLE9879QXA40 for Arduino. I already updated the firmware to make setParameter() work.
The motor works when I do the start motor in the setup void but it doesn't not turn on when the start motor is in a void loop. The LEDs blink correctly in the void loop, but the motor doesn't do anything.
How to I get the motor to work in the void loop?
Dear Infineon Comunity,
I am working on a project with the TLE987x microcontroler. Now I am using the TLE987x EVAL-Board with the spring socket. TLE987X EVALB_VQFN
I would like to ask about the feasibility of independently shifting CCU6 PWM signals. I am currently investigating ways to integrate PWM Phase Shift Compensation.
The Phase Shift Compensation should be capable to shift one PWM signal to the right, another to the left, while keeping the third signal unshifted would be beneficial.
For additional details and visuals, please refer to the document link provided on page 18.
Sensorless-FOC for PMSM With Single DC-Link Shunt (ti.com)
I hope that the community can answer my question.
Best wishes,
Stefan
How to obtain the multi-function power development kit and related materials
Hi
I'm trying to find out if these chips have a unique ID. I know that there is an ID, but is it unique? In other words is there a Chip Serial Number? Where it is described and how can be accessed (read) at run and or programming time?
Best Regards,
Tenko Yavashev
Show LessHello Team,
We are controlling a DC motor over LIN. We used the "BDRV_EMO_DC_LIN_EXAMPLE_TLE986X" package as our base.
We are also measuring the current through CSA. The SOC is triggered by a Timer3 OF interrupt.
additionally we need to used some ADC channels to read some external sensor signals.
Although when we enable interrupts for ADC channels, other CPU tasks like LIN are affected. the LIN gets totally stopped.
It seems the CPU is always falling into ADC interrupt. We tried changing ADC clock and sample time, but no success.
Show Less
Please tell me, when I use the Config Wizard for MOTIX MCU 987X software to open ICW_TLE987x.xml and config.icwp, I get the following error
Does anyone know why this is?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/%E5%85%B3%E4%BA%8E-Config-Wizard-for-MOTIX-MCU-987X/td-p/637153
Show LessHi, I'm writing a piece of software to check whether certain conditions are met in order to "reboot" the microcontroller (like you would reboot your desktop OS to "start over"). How would I do that on a TLE9893 microcontroller?
Thanks in advance.
Show LessHello:
The problems we encountered in the debugging of the TLE9891/TLE9893 chip project are as follows: When our app program enters through BOOT, the situation is normal, but the power is turned on again after power loss, the MCU will report two faults, CSC_OC_IS and WD_FAIL_STS, causing the motor to not be driven. After trying to use a register to clear the fault state, the fault still exists. (If you don't boot into the app, there will be no problem)
The following registers have been cleared:
CSC_OC_ISC
WD_FAIL_STS_CLR
FSWD_RST_CLR
The following troubleshooting has also been carried out, but the fault still exists
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOTIX-MCU/TLE9893-%E6%8A%A5CSC-OC-IS%E5%92%8CWD-FAIL-STS%E4%B8%A4%E4%B8%AA%E6%95%85%E9%9A%9C/td-p/637155
Show Less