MOTIX™ MCU Forum Discussions
Want to have the development kit of TLE9842 MCU.
Please suggest for the same like link to purchase, lead time as I am not able to get the details for this part number
It is urgent pls look into it
Show Less
Hello team,
I am using TLE9869QXA20 customized board which does not have internal debugger for my application can I use ULINK2/ME cortex debugger for debugging. If yes, can you please help me with the interface and connection with the customized board and also the settings I have to make in keil application for debugging.
Show LessDear Infineon Comunity,
I am working on a project with the TLE987x microcontroler. Now I am using the TLE987x EVAL-Board with the spring socket. TLE987X EVALB_VQFN
After reviewing the user manual, I encountered difficulties while integrating the ADC.
I would like to ask about the feasibility of an triggered ADC which measures three times a voltage. After the three measurements an interrupt is requested. I think this might be achievable through DMA or a similar hardware interrupt mechanism such as a ADC queue.
I hope that the community can answer my question.
Best wishes,
Stefan
使用官网的BLDC_BC_BEMF_EXAMPLE_TLE9879X,在Emo_StartMotor函数里面设置的是6极电机,我想改成8极,直接修改 angle6 = 6 * (uint32)Emo_Bemf.StartAngle;这个参数不太对。请问是还有其它相关联参数要写吗?
I bought a 12V Motor Control Kit, and I found the demo in-flash is very useful.
Please give me a hand let me know how to get the demo code,
Thanks a lot!
Show LessI have the BLDC motor shield with TLE9879QXA40 for Arduino. I already updated the firmware to make setParameter() work.
The motor works when I do the start motor in the setup void but it doesn't not turn on when the start motor is in a void loop. The LEDs blink correctly in the void loop, but the motor doesn't do anything.
How to I get the motor to work in the void loop?
Dear Infineon Comunity,
I am working on a project with the TLE987x microcontroler. Now I am using the TLE987x EVAL-Board with the spring socket. TLE987X EVALB_VQFN
I would like to ask about the feasibility of independently shifting CCU6 PWM signals. I am currently investigating ways to integrate PWM Phase Shift Compensation.
The Phase Shift Compensation should be capable to shift one PWM signal to the right, another to the left, while keeping the third signal unshifted would be beneficial.
For additional details and visuals, please refer to the document link provided on page 18.
Sensorless-FOC for PMSM With Single DC-Link Shunt (ti.com)
I hope that the community can answer my question.
Best wishes,
Stefan
How to obtain the multi-function power development kit and related materials