Motor Control ICs Forum Discussions
Hi everyone,
I want to show the motor voltage to the users, and for that i will use the MotorVoltage register.
I am having a bit of problem with the conversion from codes to V RMS.
The Max_Vdcsense is 500V so, using this formula, when the codes are 4974 the motor voltage is approximately 118 V RMS.
But i am using an triphasic induction motor (230V 50Hz), and in the script Induction motor control by iMOTION™ (infineon.com) the max Vq_Ext = 4974, but the max voltage in each phase should be 230V, right?
I would apreciate some clarification.
Best Regards,
Paulo
Show LessHi,
In previous version (MCE Designer) we could combine script file and parameter file and firmware file . Can we combine "out.ldf" and other "IMC102_FO64.ldf" file in iSD? and can we use MCE Designer to program the MCU(imc102) with the combined output file of iSD?
is there a software that could program the MCU(imc102) without the accessibility to configuration parameters?
how can we lock the MCU(imc102) with iSD?
Thanks
Show LessHi,
Do we have a motor control plus PFC solution in a single microcontroller?
Thanks,
你好,
我使用ModusToolbox的launch Project Creator下载了关于EVAL_IMD700A_FOC的Keil工程,其中的XMC FOC 3 Shunt例程编译无法通过,下图是报错,但是双击报错没有跳转出报错的代码位置,不知道该怎么改。
我把例程放到附件中了,希望能够得到帮助,谢谢。
Show LessCustomer had a problem with EVAL M1 301F using Version 6.21 arm compiler. The below picture shows the L6236E error from an example project from Infineon site run on Keil.
Show Less
Hi everyone,
I want to check if the input current when the PFC is ON normally has this spikes.
The spikes appear when there is no motor running, they happen with the osciloscope connected and disconnected.
Motor OFF
Motor ON
I tunned the PFC parameters to get a better current waveform.
After seeing this problem with the new parameters i also checked with the parameters before the tunning, and happened the same.
Motor OFF - NO PFC TUNNING
Motor ON - NO PFC TUNNING
What can cause this?
Best Regards,
Paulo
Show LessHi Infineon.
We had designed Ecu Based on TLE987. Now we need bootloader for reprogramming. But to Develop a new bootloader start form zero is a big challenge for us. we want a bootloader demo based on TLE987. thanks a lot!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/How-do-I-learn-Bootloader-of-TLE987/td-p/713823
Show Less
Good morning all,
I got an issue when I try to flash with iMotion Solution designer and IMotion link , two IMC302 on three prototypes, one is working.
- My 5V00 is perfect with decoupling capacitors for each power pins, tested also with a laboratory power supply & iMotion link (3V3 out)
- Tested with strong pull up 3K, added on RX, TX pin
With Salaea analyser I can recordered this :
@57600 Bauds
Imotion Link -> 0x00, 0x93 Answer : 0xA2, 0x00, 0x67 0xA2 + PDIV
Imotion Link -> 0x00, 0xAA Answer : 0xF0 PDIV + OK
@1000000 Bauds
Imotion Link -> 0xA0, 0X20, 0x00, 0x00, 0x82 Answer : 0x90
Imotion Link -> 0xA0, 0x00, 0x00, 0x01..............0x73 Answer : 0x90, 0x00
Imotion Link -> 0xA0, 0X20, 0x00, 0x00, 0x82 Answer : 0x20
Imotion Link -> 0x47, 0x2C, 0x0F, 0x7C..............0x73 Answer : 0x69, 0x82
And now IMotion Solution Designer says : Error while programming.
I would like also some support to programm the IMC302A with Segger trough SWD, I can connect, I can erase the uC, but what is the way to program the output files : IMC302A-F048_A_V5.02.00.ldf & out.ldf ?, the segger tools whant to have a .bin or a .hex file.
It is a very important project for me and my compagny, could you give me more information what could arrive ?
In advance thanks a lot for your support and help.
Best regards
Show LessHello, I have 2 questions related to the current measured signal in EVAL-M1-IM323 and e EVAL-M1-101T:
1. I wondered what is meant by internal x3 gain? is that mean inside the software?!
2. what is the benefit from the 2K ohms resistors connected between IU-, IV-, IW- and ground?
attached the schematic of controller board EVAL-M1-101T.
Thanks!
Show Less