Sep 29, 2021
12:38 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 29, 2021
12:38 AM
Why is the power-on reset bit of the global status byte active low at the TLE92104 and TLE92108?
Unlike the other status bits of the global status byte, the (negated) power-on reset (NPOR) bit is active low:
- NPOR = 0 after a power-on reset of the device. NPOR stays 0 until GENSTAT is cleared
- NPOR = 1 if GENSTAT is cleared
The arbitrary polarity definition of this bit allows the microcontroller to detect a shorted SDO line to GND: After a clear command on GENSTAT, NPOR should be 1(the power on-reset is “cleared”), unless SDO is shorted to GND.
If the SDO line is shorted to GND or the device is in sleep mode, then the microcontroller reads NPOR = 0, despite the attempt to clear the GENSTAT register.
Note: The microcontroller can detect a short circuit to VDD if the most significant bit (MSB) of the Global Status Register is set. Indeed, according to the SPI protocol of the TLE92108/4, the MSB of the Global Status Register must be 0, unless the SDI line is shorted to VDD.
Unlike the other status bits of the global status byte, the (negated) power-on reset (NPOR) bit is active low:
- NPOR = 0 after a power-on reset of the device. NPOR stays 0 until GENSTAT is cleared
- NPOR = 1 if GENSTAT is cleared
The arbitrary polarity definition of this bit allows the microcontroller to detect a shorted SDO line to GND: After a clear command on GENSTAT, NPOR should be 1(the power on-reset is “cleared”), unless SDO is shorted to GND.
If the SDO line is shorted to GND or the device is in sleep mode, then the microcontroller reads NPOR = 0, despite the attempt to clear the GENSTAT register.
Note: The microcontroller can detect a short circuit to VDD if the most significant bit (MSB) of the Global Status Register is set. Indeed, according to the SPI protocol of the TLE92108/4, the MSB of the Global Status Register must be 0, unless the SDI line is shorted to VDD.
Labels
- Tags:
- IFX
0 Replies