MOTIX™ Driver

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
User22801
MOTIX™ Driver
TLE9210x - What is the value of CSA1L field in a situation where Rshunt is in series with motor and motor changes rotation direction?1. In a situation... Show More
User22801
MOTIX™ Driver
The static charge current ICHGST and the static discharge current IDCHGST for static activation are used for two purposes:1. These currents are used t... Show More
User22801
MOTIX™ Driver
How to treat unused gate drivers when the static brake or the VS overvoltage brake are used for the TLE9210x product family?SHx must be connected to G... Show More
User22801
MOTIX™ Driver
The exposed pad and the substrate of the die are connected through a non-conductive glue.This exposed pad is there for cooling purposes only to allow ... Show More
User22801
MOTIX™ Driver
There is no risk in driving VDD and EN pin together from a single microcontroller I/O pin, since when EN =0 device is in Sleep mode and there is no ac... Show More
User22801
MOTIX™ Driver
Rotation from HS1 to LS2:1. SPI FRAME: 0b 1100 1101 0000 0000 0000 0110 – HB1MODE = 10b HS1 ON – HB2MODE = 01b LS2 ON2. SPI FRAME: 0b 1101 1101 00... Show More
User22801
MOTIX™ Driver
Are the charge pumps of the TLE92104 and TLE92108 still working in the case of fault condition?In case of a fault on a half-bridge driven by the devic... Show More
User22801
MOTIX™ Driver
Is it possible to independently drive HS and LS stages of a single half-bridge for the TLE9210x?The HSx and LSx outputs of a single half-bridge cannot... Show More
Forum Information

MOTIX™ Driver

The MOTIX™ Driver forum is designed for you to post your questions, comments and feedback about multi MOSFET driver ICs and motor gate driver ICs at anytime. Ask your technical questions or explore existing content!