Fault current on IS pin in BTN7030-1EPA?

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User21776
Level 1
Level 1
First question asked
In what situations is there fault current on IS pin in BTN7030-1EPA?
0 Likes
1 Solution
User19575
Level 3
Level 3
10 replies posted 5 replies posted First question asked
There are number of situations in which the value of the current on IS pin signals that a fault condition is met. In this case there is no following of the output current value. These are all situations in which internal latch = 1 and DEN = HIGH and one of the following situations occur:

o Short circuit to GND (HS switch)
o Short circuit to Battery (LS switch)
o Overtemperature on HS or LS switch
o Overcurrent on HS or LS switch
- For more information please refer to https://www.infineon.com/dgdl/Infineon-BTN7030-1EPA-Diagnosis-and-Protection-ApplicationNotes-v01_00...

View solution in original post

0 Likes
1 Reply
User19575
Level 3
Level 3
10 replies posted 5 replies posted First question asked
There are number of situations in which the value of the current on IS pin signals that a fault condition is met. In this case there is no following of the output current value. These are all situations in which internal latch = 1 and DEN = HIGH and one of the following situations occur:

o Short circuit to GND (HS switch)
o Short circuit to Battery (LS switch)
o Overtemperature on HS or LS switch
o Overcurrent on HS or LS switch
- For more information please refer to https://www.infineon.com/dgdl/Infineon-BTN7030-1EPA-Diagnosis-and-Protection-ApplicationNotes-v01_00...
0 Likes