Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

PaulojM
Motor Control ICs
Hi everyone, I want to show the motor voltage to the users, and for that i will use the MotorVoltage register. I am having a bit of problem with the c... Show More
Mahimc2020
Motor Control ICs
Hi, In previous version (MCE Designer) we could combine script file and parameter file and firmware file . Can we combine "out.ldf" and other "IMC102_... Show More
oscarkeser01
Motor Control ICs

Hi, 

Do we have a motor control plus PFC solution in a single microcontroller?

 

Thanks,

 

Xuehs
Motor Control ICs
你好,   我使用ModusToolbox的launch Project Creator下载了关于EVAL_IMD700A_FOC的Keil工程,其中的XMC FOC 3 Shunt例程编译无法通过,下图是报错,但是双击报错没有跳转出报错的代码位置,不知道该怎么改。   我把例程放到附件中了,希望... Show More
oscarkeser01
Motor Control ICs
Customer had a problem with EVAL M1 301F using Version 6.21 arm compiler. The below picture shows the L6236E error from an example project from Infine... Show More
PaulojM
Motor Control ICs
Hi everyone, I want to check if the input current when the PFC is ON normally has this spikes. The spikes appear when there is no motor running, they ... Show More
Translation_Bot
Motor Control ICs
Hi Infineon. We had designed Ecu Based on TLE987. Now we need bootloader for reprogramming. But to Develop a new bootloader start form zero is ... Show More
micheldurand
Motor Control ICs
  Good morning all, I got an issue when I try to flash with iMotion Solution designer and IMotion link , two IMC302 on three prototypes, one is workin... Show More
Kaleeswaran
Motor Control ICs
Hello all we tried the imc101t-f048 controller for driving the BLDC motor(achieving 3000rpm in 2 seconds), but we could not achieve this using both th... Show More
Ahmed_Kamal22
Motor Control ICs
Hello, I have 2 questions related to the current measured signal in EVAL-M1-IM323 and e EVAL-M1-101T: 1. I wondered what is meant by internal x3 gain?... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.