May 07, 2021
04:29 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 07, 2021
04:29 AM
Is it possible that one microcontroller I/O port drives two EN pins of two different BTN7030?
Are there any limitations?
Are there any limitations?
- Tags:
- IFX
1 Reply
May 10, 2021
12:39 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 10, 2021
12:39 AM
From a functional perspective, there is no limitation.
There is no problem as far as the uC I/O can handle the 2 x pull-down currents of EN pins.
These currents are max. 25 µA (Novalite DS), so sinking/sourcing should not be an issue for the GPIO of the uC.
There is no problem as far as the uC I/O can handle the 2 x pull-down currents of EN pins.
These currents are max. 25 µA (Novalite DS), so sinking/sourcing should not be an issue for the GPIO of the uC.