Not applicable
Mar 07, 2017
04:53 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 07, 2017
04:53 AM
Hello,
I am reading the data sheet of IRS2113. And something come to my mind:
What is the definition of Allowable offset supply voltage
transient?
Thank you!
I am reading the data sheet of IRS2113. And something come to my mind:
What is the definition of Allowable offset supply voltage
transient?
Thank you!
Solved! Go to Solution.
- Tags:
- IFX
1 Solution
Not applicable
Mar 07, 2017
05:58 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 07, 2017
05:58 AM
It is the maximum rate at which the voltage at the VS pin can change is 50 V/ns. This high degree of tolerance makes the IC robust, and ensures excellent device performance in demanding applications such as motor drives, switching power supplies, etc. The dVS/dt capability is measured as per the test set up shown in Fig. 2 of the datasheet: https://www.infineon.com/dgdl/irs2110.pdf?fileId=5546d462533600a40153567660ff27b0
1 Reply
Not applicable
Mar 07, 2017
05:58 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 07, 2017
05:58 AM
It is the maximum rate at which the voltage at the VS pin can change is 50 V/ns. This high degree of tolerance makes the IC robust, and ensures excellent device performance in demanding applications such as motor drives, switching power supplies, etc. The dVS/dt capability is measured as per the test set up shown in Fig. 2 of the datasheet: https://www.infineon.com/dgdl/irs2110.pdf?fileId=5546d462533600a40153567660ff27b0