difference between RthJC and RthJA

Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
What is the difference between RthJC and RthJA? We see the same value of Rthjc for CoolMOS TO247 package, CoolMOS DPAK and CoolMOS IPAK
0 Likes
1 Solution
yifei_y
Moderator
Moderator
Moderator
250 replies posted 25 likes received 100 solutions authored
RthJC is the thermal impedance between Junction to Case. This is the same irrespective of the package type, except for Full PAK where the mold compound is different / thicker adding thermal impedance. Hence except Full PAK, the remaining packages have the same Rthjc. SOT223 is also an exception, considering a very small package structure. This does not include the heat sink.

RthJA is the thermal impedance between Junction to Ambient. This includes the heat sink. Hence based on the standard heat sink assembly used during device characterization, the RthJA of different packages are different.

View solution in original post

1 Reply
yifei_y
Moderator
Moderator
Moderator
250 replies posted 25 likes received 100 solutions authored
RthJC is the thermal impedance between Junction to Case. This is the same irrespective of the package type, except for Full PAK where the mold compound is different / thicker adding thermal impedance. Hence except Full PAK, the remaining packages have the same Rthjc. SOT223 is also an exception, considering a very small package structure. This does not include the heat sink.

RthJA is the thermal impedance between Junction to Ambient. This includes the heat sink. Hence based on the standard heat sink assembly used during device characterization, the RthJA of different packages are different.