Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

MOSFET (Si/SiC) Forum Discussions

Rakesh_rp
MOSFET (Si/SiC)
Hi, I have a doubt in  3.3kW PFC stage  in the given Infineon code for 3.3kW PFC demo board.  The VIN AC RMS voltage is calculation is done by using a... Show More
ckeeltd
MOSFET (Si/SiC)
Hello! I am going to purchase some sample of IPN80R900P7 MOSFET for our LED lighting design project. But it is unable to source it in the current mark... Show More
jiaoleiming
MOSFET (Si/SiC)
Hi, I notice that IFX released a series of mosfets with top-side-cooling package, such as TOLT, DDPAK and QDPAK. Since the top surface should be attac... Show More
MS_19060803
MOSFET (Si/SiC)
いつもお世話になっております。 IPL60R140CFD7のSpiceモデルを用いて、シミュレーションを実施しております。 実際のデバイスでは2ピンDriver Sourceピンが存在します。 しかし、SpiceモデルにはDriver Sourceピンが存在しません。 そこで質問ですが、Spiceモ... Show More
User20393
MOSFET (Si/SiC)
Hi Regarding to EVAL_3K3W_TP_SIC I'm trying to change the dead time thru below GUI. the prolem are: 1) I have no idea what is the actual time (ns) of ... Show More
ashwani
MOSFET (Si/SiC)
Hello  Recently I purchased the Evaluation board EVAL_3K3W_LLC_HB_CFD7 it gives the output voltage  between 43.5 volt to 59.5 volt. Along with the boa... Show More
Y_Konno
MOSFET (Si/SiC)
Hi, Please send the following characteristics of IRF7306TRPBF. (1)Drain current vs. Drain-source voltage -4 V or less. The following is desirable.. (... Show More
GrCa_1363456
MOSFET (Si/SiC)
Does Infineon offer ESD ratings for their power MOSFETs? If so, where would that information be found? I'm specifically asking about N-Channel Power M... Show More
User19535
MOSFET (Si/SiC)
  Dear Sir, we are intreated in this 48V BSG inverter. could provide the Gerber file & related material, we would like to follow this kit to build up ... Show More
Cookie123456
MOSFET (Si/SiC)
  Hi  contributors,    We have a question the BSC010N04LS  parts, is there have DC :2136+will have different  marking font  and  positioning hole also... Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.