Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

MOSFET (Si/SiC) Forum Discussions

KeTs_2342536
MOSFET (Si/SiC)
Hi,   Have we IRF7342PbF SOA Maximum Safe Operating Area chart or figure for design reference? Regard, Kevin Show More
DarkKnighter
MOSFET (Si/SiC)
Hello everyone, I hope that you can help me. I guess I have a problem to understand something. For my simulation in PLECS I want to define the "therma... Show More
dommychen
MOSFET (Si/SiC)

where is wafer production location for this part number? IAUT150N10S5N035

Ahmed
MOSFET (Si/SiC)
My question is about the the reference design (VD_1000W_GAN_PSFB_XDP).  (Reference design board-1000 W, 400 V phase-shifted full-bridge current-double... Show More
thsie94
MOSFET (Si/SiC)
Hi all!  For a clearance and creepage analysis I need a cad-model of the HybridPACK Drive FS03MR12A6MA1B, most important is that the bus-bars are sepa... Show More
sgupta303333
MOSFET (Si/SiC)
Hello, I received the BSC026N08NS5STMA1 Mosfet with the following date code: 2016 Could you please tell me about the format of the date code and the s... Show More
Marty
MOSFET (Si/SiC)
PCB Engineer
solved msg Solved
Hello,  I am looking for accurate 3d models PG-TO263-7-1 and PG-TO252-3-11.The 3d models in the downloadable CAD libraries are too simplistic.Isn't th... Show More
Heatace7
MOSFET (Si/SiC)
Hi, I am only a rising senior in my university, so I am pretty new to this field beside electronics 1 and 2. Basically, I have a project that uses one... Show More
TomL
MOSFET (Si/SiC)
Dear Community, From manufacturing point-of-view, can a TDSON-8 package (eg. BSC032N04LS) be reliably solder over a TDSON-8 FL footprint (eg. BSC059N0... Show More
cooper
MOSFET (Si/SiC)
Dear , Q1:the part number IPP60R099P7XKSA1,  what is the mean of PN suffix “XKSA1” ?   Is it production batch ?  is there refered file about suffix ? Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.