Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

MOSFET (Si/SiC) Forum Discussions

Pradikrc
MOSFET (Si/SiC)

Does Wuxi fire accident has impact on D2PAK MOSFET IPB048N15N5LF?

Why is this part so expensive ?

tejesh
MOSFET (Si/SiC)
I would like to use the mentioned Gate-Driver and MOSFET for the Double Pulse Test using a Function generator. As I am designing it for the first time... Show More
goran
MOSFET (Si/SiC)
Hi Looking for datasheet power mosfet (marking NE22 from IR) also known like 94-2608, used in "Curtis" dc motor driver/controller 1244 (also obsolete)... Show More
jmchest
MOSFET (Si/SiC)
Looking for the recommended footprint for the SMD-0.2 as well as the SMD-0.5. I found the updated package details and the design note about slightly e... Show More
Carmen_MC
MOSFET (Si/SiC)
Hi, Could BSC030N08NS5ATMA1 supports up to 20A application? Current EVB using 8 MOSFETs for 10A, is higher drain current and power MOSFET needed to dr... Show More
vinloong
MOSFET (Si/SiC)
Hello all, I am trying to setup a simulation with the Spice model of the SiC MOSFET IMZA120R020M1H_L3 provided. After running the simulation I get an ... Show More
Sorakrai
MOSFET (Si/SiC)
Dear Infineon team,      Did you have EMC test reults for Eva board EVAL_3K3W_TP_PFC_SIC? Thank you. Sorakrai Show More
ra_dzik
MOSFET (Si/SiC)
Hello, I'm looking for a replacement of component marked as IOR P544H G6B8 F7017 (no sure 7017 or 7x17) - like on the picture. Could you help me to id... Show More
Red
MOSFET (Si/SiC)

I registered REF-DAB11KIZSICSYS, but I can't find the source code of XMC4400, can you upload it?

Red
MOSFET (Si/SiC)
I registered EVAL_800W_ZVS_FB_CFD7, but I can't find the source code of XMC4200 that it only has hex firmware image, can you upload source code? Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.