MOSFET (Si/SiC) Forum Discussions
What is the Infineon Package name?
The Infineon Package name of the ISC104N12LM6 is "PG-TDSON-8", but it is further classified by version, such as PG-TDSON-8-46.
For example, the link destination of "PG-TDSON-8" in the ISC230N10NM6 is "PG-TDSON-8-907 | SuperSO8 5x6" and the version can be determined, but there is no link to the ISC104N12LM6 and some part numbers.
What is the version of the PG-TDSON-8 in ISC104N12LM6?
Also, how can a part number without a link destination determine the version?
I'm sorry for the detailed question, but I would appreciate it if you could confirm.
Fujioka/Nexty
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/Infineon-package-name-PG-TDSON-8-%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6/td-p/701780
Show LessI am looking for accurate 3d models PG-TO263-7-12. Can this be provided?
Best Regards, Hari
お世話になります。
基本的な事ですが教えてください。
IMYH200R024M1Hの裏面のヒートシンクはアクティブでドレインでしょうか。
データシートに記載がないので質問させていただきました。
Hello Infinion Power Forum,
I have a question regarding measurements I made on my 3-phase inverter. I use 4 IRF100B201 Mosfets per switch for my inverter. The gates are isolated and switched with +-15 V. The gate resistance is 10 Ohms. I perform a U-turn with 20 A and measure the drain-source voltage of the high-side and low-side Mosfets. I measure negative drain-source voltages ranging from 6.9 to 11 V and am now concerned that my Mosfets may break down when increasing the current. Currently, I use a BLDC motor as a load with a stator resistance of 20 mOhm and 1uH, but I intend to switch to a stronger motor with a stator resistance of 2 mOhm and 68 uH. Could there be a measurement error here, or what would be the next steps to increase performance?
Show LessHow to calculate transformer losses and inductor losses for high frequency DC-DC converter, like DAB configuration?
Please help me in this regard
Show Less
Hi, we wish to design 6KW isolated DC-DC boost converter
input-24V
Output-96 to100V
power 6KW
MOS drive shutdown delay what model can be simulated ah
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/MOS%E7%9A%84%E9%A9%B1%E5%8A%A8%E5%BB%B6%E6%97%B6%E9%97%AE%E9%A2%98/td-p/689379
Show Less我们采购贵司的一款MOSFET 650VCoolMOS™CEPowerTransistor (型号是IPA65R400CE )现在用于我们公司的产品中,前段时间我们产品做安全认证,这款MOSFET 被认定为关键零部件,需要提供相应的UL/VED的认证证书号码,我在认证网站上没有查询到这款产品,可否提供一下,非常感谢!
Show LessHi,
I was wondering if there are radiators sold that clip directly onto the PG-HDSOP-22 package .
That would make cooling a lot easier than designing something of my own.
Thanks a lot,
Cheers
Philipp
Show Less