MOSFET (Si/SiC) Forum Discussions
Dear Sir,
I have question about Crosstalk in Totem Pole PFC.
In positive cycle, why the Vgs crosstalk of Q2 event just happen in SR Q1 turn on and turn off?
PWM FET turn on / off no induce vgs crosstalk on vgs of SR FET Q1.
Green trace: choke current
purple: Vgs of Q2
yellow: AC line @ 90 dergee
Show Less
Dear Team
so sorry to bother you
we purchased the parts from authorized distributor,
But we found that the lable in 3p section is 11 digital number, but according to the date sheet, the it's 8 digital number
could you help clarify what’s the reason for that? Any pcn are available?thanks
Show LessI have been measuring SiC MOSFET with EVAL_PS_DP_MAIN and the daughter board. But it currently not good since there is very noisy from waveform. But I noticed it became better after I connected shunt to Id150 point in mother board. So I'd like to confirm to do better measurement.
The things to be checked are following 2 points.
1.Is this circuit required to set shunt or jumper in on Id150 to implement correct measurement? It's described in attached "Infineon-Schematics_EVAL...".
2.The reason why 4 resistors are connected to capacitors between HV_VDC and GND. Is these used as RC snubber? This is described in attached "SiC-MOSFET_EVAL Board.pdf".
If there is a quesiton, please let me know.
Best Regards,
Shibata@Nexty
Show LessDear technical support team of Infineon™,
Hello,
I am slightly confused by the following data on the following datasheet for BSC026NE2LS5:
What is the difference between these two values? Why do they contrast this much?
Thank you!
Show Lessいつもお世話になっております。
過渡熱抵抗に関して質問がございます。
BSS225のデータシートにはZthJAが記載されていますが、
ZthJC(ジャンクション-ケース)のデータ提供は可能になりますでしょうか?
色々とMOSFETを確認しますと、データシートにZthJC 又はZthJAが記載されておりますが、
区別している理由がございましら、ご教示頂けませんでしょうか?
以上、よろしくお願いいたします。
Show Lessいつもお世話になっております。
MOSFETのESDについて質問がございます。
下記4デバイスのESD(Machine Model、Human Body Model、Charged Device Mode)を
ご教示頂けませんでしょうか?
・IRF7341TRPBF
・IRF7343TRPBF
・IRFR9024NTRLPBF
・IRFR024NTRPBF
全デバイスのProduct Qualification Reportを確認致しましたが、ESDの記載はございませんでしたので、
ESDは実施していないと認識しております。
もし、実施しているのでばれば確認する方法もご教示頂けましたら幸いです。
以上、よろしくお願いいたします。
Show Lessいつもお世話になっております。
IRLR3410のRθJA測定条件に関して、ご質問がございます。
データシートにはWhen mounted on 1" square PCB (FR-4 or G-10 Material )と記載されており、AN-994を参照したのですが50℃/Wに該当する条件がございまでんでした。
AN-994
↓
https://www.infineon.com/dgdl/AN-994J.pdf?fileId=5546d46256fb43b301574c600ad87c2c
1インチ(正方形)のPCBでの測定まではわかるのですが、何層、何oz(銅厚)であるかご教示頂けますでしょうか?
以上、よろしくお願いいたします。
Show Less
What are the differences between the industrial IPP65R110CFD and the automotive IPP65R110CFDA?
Are these devices coming from the same fab/process, final assembly & test? Any material differences? The only difference is the testing qualification JEDEC vs. AEC?
Thank you!
Show Less
Hi,
In IMZ120R060M1H datasheet, pin 2 & 3 are connected together.
In application, how to connect these two pins in the layout? Can tie these two pins together?
Show Less