Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

MOSFET (Si/SiC) Forum Discussions

lellone54206
MOSFET (Si/SiC)
Dear Infineon team,I'm a MSc Student at Polytechnic of Turin doing a Thesis in cooperationwith an important Aerospace Company to develop models for So... Show More
yuyj
MOSFET (Si/SiC)
IRFP4227PBF
solved msg Solved

IRFP4227PBF  ESD等级是多少,另外IMBG120R030M1HX   ESD等级多少

谢谢!

zain
MOSFET (Si/SiC)
I bought EVAL_3K3W_BIDI_PSFB evaluation board and got the exclusive access of the files. I understood the hardware design and somehow the software imp... Show More
rstaf
MOSFET (Si/SiC)
I am running a thermal analysis and am looking for the maximum junction temperature for IPT008N06NM5LFATMA1 along with the thermal resistance of the j... Show More
jmrey
MOSFET (Si/SiC)
Hello, I would like to know if the source code of the KIT_600W_LLC_DI_CTRL is available somewhere, or if it's only a evaluation board to test the digi... Show More
satwik
MOSFET (Si/SiC)
Hello all, I am trying to setup a simulation with the Spice model of the SiC MOSFET IMW120R040M1H_L3 provided. After running the simulation I get an S... Show More
MS_19060803
MOSFET (Si/SiC)
いつもお世話になっております。 基本的な質問で申し訳ございません。 MOSFETは寄生サイリスタ構造を有しているかの質問になります。 色々と調べるか限り、寄生サイリスタ構造ではないと考えておりますが、 この理解は正しいでしょうか? 仕様書作成の作成のためにこの情報が必要になります。 対象デバイスはI... Show More
Desheng_Zhang
MOSFET (Si/SiC)
When assuming that the heat dissipation condition is excellent, so that the temperature of SiC Mosfet in the inverter is within a reasonable range, ca... Show More
zhuxiaozhu
MOSFET (Si/SiC)
hello dear, I'm working at Halfbridge LLC But he square wave spike of the half-bridge output is too large (20V input, the peak is up to 35V)  the vol... Show More
Edgar_Jiang
MOSFET (Si/SiC)
hi I want to know the difference between IPD50P04P4L11ATMA1 and IPD50P04P4L11ATMA2.My client want to order IPD50P04P4L11ATMA1,but we only have  IPD50P... Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.