MOSFET (Si/SiC) Forum Discussions
Dear IFXer,
I would like to discuss why dynamic parameter Ciss, Cgd, Coss, Qg, Qgd, Qds are no marking min and max value in datasheet? In all power device vendor? Thus, how to consider design in worst case?
and further question is the IMZA can co-layout with IMZ package ? if it is possible, what is our consideration in layout?
Show Less
Hello, I need some data when using FF6MR12W2M1_B11, these data can not be found in the data sheets, hereby ask: does the product have a corresponding curve of capacitance and Vds (Capacitance vs Vds), Rdson and temperature change curve (Rdson-Junction Temperature), gate charge Qgs, Qgd value under typical working conditions? Looking forward to hearing from you.Have a good time!
Show LessHi all,
BSZ096N10LS5のコプラナリティは何mmですか?
データシートで見つけられませんでした。
How many millimeters is the coplanarity of BSZ096N10LS5?
I couldn't find it in the datasheet.
Best regards,
MS
Hi,
May i know is the part no BSP300H6327 can replace BSP300 part no ?
And what is the difference between these 2 parts ?
Many thanks with kind regards,
Song.
Show LessHello,
I was having a conversation with Rishav on bare-die devices. For some reason, I cannot reply to that conversation now. Can I have a list of bare-die MOSFETs that we can buy from Infineon?
Sajal
Vanderbilt University
Show LessHello Team,
i am using the depletion Mosfet BSP129 for the High voltage protection . the gate of the Mosfet is tied with the Zener diode of 11V and expecting the output to be stabilize till Vz + Vgs of the Mosfet. also at the source i have connected Comparator circuit which will detect at 10.5V for further processing. before connecting this TL431 Comparator circuit the response was ok. but when i am connecting high voltage i am getting oscillation on the source of the Mosfet and its getting settle down after few hundreds of ms. but that is not expected that should be settle in less than 50us. this behavior is observed specially on -40 degree.
please let me know if any suggestion ??
below i have attached few waveform and Simulation schematic.
Show LessHello IFXer,
May I know the SIC driver board for hybirdpak has refereance schematic? and I would like to know how to simple check issue if the driver board has abnormal event?
HPD GD BOARD G1 SIC - Infineon Technologies
Show LessHello All,
Can somebody please help me?
I would like to know about the IPW60R040CFD7 if the Tab and the Drain are isolated.
In the datasheet, an insulation withstand voltage is mentioned (but not measured), what does it relate to?
I have observed on datasheets, in most of the cases when Drain and Tab are connected, it can be
directly seen from the schematic of the MOSFET.
kind Regards,
Show LessWhich capacitance parameters need to be taking care if we compare the mosfet capacitance parameters that affect the radiared EMI performance? (eg, Coer or Cotr and Output capacitance and so on)
Show Less