Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

MOSFET (Si/SiC) Forum Discussions

ydhote44
MOSFET (Si/SiC)

hello, can somebody guide me where i can get verilog-A code of cypress depletion model mosfet (level 38 mosfet ).

sen789
MOSFET (Si/SiC)
Hi, I would like to know which type of this company's SiC MOSFET product has multiple bonding wires and the case can be opened by chemical etching. I ... Show More
yjc0101
MOSFET (Si/SiC)
HI. As shown in the figure below, I would like to know how the 30A current is calculated for the IAUC120N06S5N017 at T a=85 °C, VGS=10 V,RthJA on 2s2p... Show More
achim
MOSFET (Si/SiC)
Hi, I´ve to design an (static, no PWM) switch for 60V / 200A cont. (420A peak for max. 10s). I consider the IPTC007N06NM5ATMA1. Is it in general bette... Show More
gm2023
MOSFET (Si/SiC)
 Hi, I am from bits pilani. We need a bidirectional CLLC converter of 10 KW which should be having Vin=600-700 and Vout=48-72 Volt, The Power output o... Show More
sunder3069
MOSFET (Si/SiC)
We would like to buy the reference  design evaluation Board , Having come to understand the boards are ready and accepting the order, To order we requ... Show More
MASK310
MOSFET (Si/SiC)
The IMBG120R350M1H is a great device, boasting one of the fastest switching speeds among SiCMOSFETs. According to the datasheet, the turn-on rise time... Show More
jumpshowhigh
MOSFET (Si/SiC)
Seems that Infineon has discontinued this part.  Any suggestions for a similar part in a 3-pin TO262 package with similar RDS-on?  The replacement is ... Show More
sunnysky
MOSFET (Si/SiC)
MOSFET choose:IPLU300N04S4-R8 Driver IC choose:IRS2101S The fever is serious when the continuous current reaches 40A! why? How to choose the Driver I... Show More
yjc0101
MOSFET (Si/SiC)
ALL Hi. As shown in the figure below, when I use IAUC120N06S5N017 for circuit design. If the material of the PCB used is RF4, four-layer board 2S2P, c... Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.