MOSFET (Si/SiC) Forum Discussions
As the title says, do you have a full featured step model for this part ?
I am designing in Alttium.
Thank you
As there is no public information yet on the M1H MOSFET modules, can someone at Infineon confirm that the part numbers listed under the "M1H Replacement" will be direct pin-for-pin compatible replacements for the M1 parts which they are replacing?
The replacement list is found here: https://www.infineon.com/cms/en/product/power/mosfet/silicon-carbide/modules/
For example, the F4-23MR12W1M1_B11 is discontinued and has been replaced with the F4-17MR12W1M1H_B76. Is the pinout and package identical between these two modules?
F4-23MR12W1M1_B11 |
Sep 22 |
Fourpack |
F4-17MR12W1M1H_B76 |
Already available, webpage coming soon |
Show Less
hi all,
is the thermal model for device BSC040N10NS5ATMA1 available?
Thanks
GF
Try to replace this part direct on my board, but not able to boot up after replaced.
tried with parts below, all not working.
IRF9328TRPBF
Show LessI'm looking for a very high voltage Si FET at very low current.
The best catalog part I've been able to find is IPN95R3K7P7ATMA1
I'm looking for a part with Vds max over 1300V.
my actual current will always be less than 1.5 mA worst case
my potential quantity is moderately high 50K to 200K/ year
do you have anything and or might they select for high Vds
from the 950V IPN95R3K7P7 parts??
Show Less
Dear Team,
Is CoolMOS SOT223 products (eg: IPN60R600PFD7) wave-soldering compatible? An appnote or KBA reference will be much appreciated.
Thanks,
Bob
Show Less
I need to make a Resonant Inverter, with AC output.
- application is an AC power supply
- Topology: LLC or other
- Input: 12V to 24V DC
- 100 kHz
- 100W
- 0 to 20A continuous
- constant voltage
- 0 to 5V
- Inductive load: Several coupled inductors. The secondaries won't be rectified.
- pure sine
- soft-switched
- 1/2 bridge or 1/4 bridge
We will not rectify or filter the output.
Our load is several coupled inductors. We won't rectify the secondaries of those load-inductors. The load requires AC power.
What Infineon parts are recommended? Seeking FET's, gate driver, controller, etc
Show LessWhy CoolSiC SiC MOSFET Vth is specified by testing after 1ms pulse at Vgs=20V
Hi all,
Please let me know about the negative voltage of the 1700V CoolSiC MOSFET.
Regarding the gate voltage, the datasheet says “please refer to Application Note AN2018-09”.
So, is it okay to use the graph below for 1700V "M1"?
Best regards,
MS