Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

MOSFET (Si/SiC) Forum Discussions

MOSFET (Si/SiC) Forum Discussions

Sort by:
User17640
MOSFET (Si/SiC)
Hi,i just read Infineon offers gate driver ICs for MOSFETs. What makes them the best choice?thank you 🙂 Show More
User17150
MOSFET (Si/SiC)
Is +15 VGS to high voltage for this NFET? Why is Qg VGS=0-10v only test VDD=100v? Is 180ns dead band enough recovery time for FD diode in 20kHz PWM? H... Show More
Fränce
MOSFET (Si/SiC)
Why should I use SiC MOSFETS? Which applications are being targeted?
User17477
MOSFET (Si/SiC)
I have constructed an H-Bridge using two IR2101S driver ICs and four IRFZ44N power FETs, it works and there are no problems.I have now been given an a... Show More
User17008
MOSFET (Si/SiC)
Hello, I want mosfets N withRDS (on) @10V max 8 mohmVBRDSS >= 30VGS(th) max 2.2 VID @ TC=25°C min 59 AQG typ @10V ... Show More
User16939
MOSFET (Si/SiC)
Good day, gentlemen, I need your help in identification, I'm interested in
VDSS = **V, RDS(on) = **mΩ, ID = **A?
User16587
MOSFET (Si/SiC)
Hello, I would like to use an infineon 600 V Power MOSFET for building up a high voltage test equipment. If the continuous drain current (Id) rating o... Show More
User15550
MOSFET (Si/SiC)
"Register Map" tab is absent in last builds of PowIRCenter software(6745 and 6774).Is the previous builds with this tab (e.g. build 6200) completely s... Show More
Anonymous
MOSFET (Si/SiC)
Hello,I am trying use the simulation models of the ir2010 driver and irfb4321 mosfet in OrCAD. Both devices show the same problem during simulation:E... Show More
User15550
MOSFET (Si/SiC)
Is it REFIN 1.8V nesessary to proper operation IR3555M with IRPS5401 in DCR sensing mode? (IOUT pin would be unused) IR3555 datasheet is extremely sho... Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.